Hi David,
Thank you for the fast repply.
Now, I am trying to simulate in LTSpice the values you told me. So based on that, I create the following model for the transformer you used for the flyback reference design. The coupling value is based on the…
Part Number: CSD18504Q5A Other Parts Discussed in Thread: CSD18511Q5A Hello,
There is recommended stencil information in the datasheets of the below two devices.
CSD18504Q5A
CSD18511Q5A
But there is no information about its stencil thickness.
Could…
Part Number: CSD18504Q5A Other Parts Discussed in Thread: CSD18511Q5A Hello,
I have a question for the bellow devices.
・CSD18504Q5A
・CSD18511Q5A
Does TI recommend to use Pad-on-Via for Drain terminal of these devices?
Do you have any recommended design…
Hi Eric, but I'm not clear, there are one low side and one high side mosfets. In the diagram I proposed to you, there are 2 identical ASDM30N55Es in both LowSide and HighSide. If I were to replace them with those suggested by Webench (which could be the…
Part Number: LM25149 Other Parts Discussed in Thread: CSD18514Q5A , CSD18504Q5A , LM5148 I'm making a design with LM25149
Design spec.: 15V to 28V input and 12V output, max current is 7.5A
I have used Webench for a design suggestion. Webench suggest …
Other Parts Discussed in Thread: CSD18504Q5A Hello.
My customer is currently in using CSD18504Q5A,now.
I have gotten a question about this product .
So, please teach me about CSD18504Q5A.
<Question>
Due to unforeseen circumstances,
does the device be easily…
Hello Kwangsug
I think there is a misunderstanding. CSD18514Q5A is 4-6mOhm, 29nC @ 10V MOSFET. CSD18504Q5A is 6=10mOhm , 15nC @ 10V MOSFET.
You can use the same MOSFETs on both high- and low-side, but usually engineers select higher Rdson & lower Qg MOSFET…
Part Number: EM1402EVM Other Parts Discussed in Thread: CSD18504Q5A , BQ79616 Hello,
We are currently building modified EM1402EVM boards for our battery system. Many of the components used are unavailable or obsolete. Do you have qualified alternatives…
Other Parts Discussed in Thread: LM3150 , CSD , TINA-TI , CSD18504Q5A , CSD18501Q5A , CSD18503Q5A I'm wondering the the CSD1850x family NexFET's are slated for TINA-TI model conversion any time soon. I noticed that quite a few of the lower voltage CSD…