Part Number: CSD18536KCS Hi Experts
Can you confirm that the information in Figure 10 is incorrect for this device?
It shows operation up to 100V is OK, but the rest of the datasheet says 60V.
Can the proper SOA diagram be provided?
Thanks!
Jim B
Part Number: CSD18536KCS Hello,
We would like to know the ESD ratings for CSD18536KCS. Could you teach us the value of HBM(MM) and CDM. We couldn't find this information in the datasheet.
Best Regards, itabi
Part Number: CSD18536KCS Hi Power Management team, Is the CSD18536KCS N-Channel FET automotive qualified? If not, can you please recommend the best automotive-qualified alternative? Thank you for your help, Manuel Chavez
Part Number: LM5117 Other Parts Discussed in Thread: CSD19505KTT , CSD19538Q2 , CSD18536KCS I am working with the LM5117 and i have failed to get the output signal to the FETS.
Below is my circuiit diagram with values computed with the LM5117 Quick calc…
Hello John,
I am actually also interested in using the same MOSFET (CSD18536KCS) to simulate my design. I am using LT-spice to simulate, and I was wondering if it's possible for me to have the model so I can import into LT-spice to simulate my SMPS circuit…
Part Number: CSD18536KCS We are designing the inverter circuit using the MOSFET CSD18536 and Driver-UCC3895.
The input voltage is 48V, the output voltage is 400V, and the circuit is being designed with a phase shift method of 300W output.
However, ripple…
Other Parts Discussed in Thread: CSD25404Q3 , TINA-TI , LM7480 , CSD18536KCS , LM5060 , CSD18536KTT , LM7480-Q1 Need to Trigger PMOS at 48V for a Source switching circuit, can you help. I was looking iinto Voltage devider as a trigger
Other Parts Discussed in Thread: CSD18536KCS Hi Team,
I am working on a low side NFET driver that needs to handle a continuous current of 50A. I am thinking of using the CSD18536KCS due to its high current capability but I have a question about Vds.
Currently…
Part Number: CSD18535KCS Other Parts Discussed in Thread: CSD18536KCS , Hi Team, May we request for the lib file for CSD18535KCS? The lib file given on the PSpice model (slpm151a) present on its product page seems to be incorrect, as it is the lib file f…
Part Number: CSD19536KCS Other Parts Discussed in Thread: CSD19506KCS , CSD18536KCS Hi Team,
A customer requests us the data of “Eoss vs VDS” for the following 3 devices. If you have any data to be able to share with customer, please support it.…