Other Parts Discussed in Thread: CSD19531Q5A , CSD18537NQ5A Hi,
We are using the following TI components in our design.
TPA3111D1PWP
LM25085SD
LM5175RHF
CSD19531Q5A
MSP430F5659IPZ
TPS7A1901DRB
CSD18537NQ5A
TPS23861PW
LM5022MM
Can…
Other Parts Discussed in Thread: CSD18543Q3A , CSD17585F5 , CSD18537NQ5A , CSD18514Q5A AO3400 is used as the load switch to control a fan, which must have 2A, 24V capacity;
wsf40n06 is used as the load switch to control the heating resistor, which must have…
Hi Yue,
The cap from CS to CSG should be lower value (1nF) and use the R9 and R12 resistors for filtering with a time constant of 10-20ns. The boot resistor can be 5-10 Ohms. Also, you can check the compensation values using the quickstart calculator…
Hello Brett,
My name is Toshio Fukumoto. Im FAE of
My Customer requests the Psi-JT and Psi-JB of CSD18537NQ5A, CSD18563Q5A, CSD18540Q5B, and CSD18532Q5B.
They want to use FETs with TPS40171 (DC/DC Controller).
Package top temperature of CSD18537NQ5A…
Part Number: LM25116 Other Parts Discussed in Thread: CSD18537NQ5A Hi there:
greeting, I'd like to have your help to double check the design idea whether is workable or not. (mainly use LM25116 firstly)
our MOSFET was choose CSD18537NQ5A*2 .
Please…
Hi Yang,
Thank for your valuable input. Actually we are replace this MOSFET DMNH3010LK3 with TI's CSD18537NQ5A MOSFET and the converter is working now.
But we cant identify which parameter of MOSFET affect so that we cant get the any output.
Part Number: CSD17573Q5B Other Parts Discussed in Thread: TINA-TI , , CSD18537NQ5A , LM5176 , CSD19534Q5A , CSD16321Q5 Tool/software: TINA-TI or Spice Models I have pulled the most recent version of the CSD17573Q5B PSpice Model from the TI web page. I am running…
Other Parts Discussed in Thread: TPS28225 , CSD18537NQ5A , CSD88539ND Hello Team,
Could you tell me whether TPS28225 can be used in Half Bridge parallel configuration or not?
I'm thinking about using CSD88539ND or CSD18537NQ5A.
Best Regards,
Hidetoshi…
Other Parts Discussed in Thread: CSD18504Q5A , CSD18537NQ5A , LM25116 , LM5116 Hi,
I had a design went through below for a 24V to 5V@15A buck a few days back.
Design : 4561043/188 LM5116MHX/NOPB
LM5116MHX/NOPB 22.0V-26.0V to 5.00V @ 15.0A
Now I ran the same…