Part Number: CSD18542KTT Other Parts Discussed in Thread: CSD18540Q5B , CSD19505KTT , LM9061-Q1 Hello Team,A. We want to select an N channel based on the following specifications.
90A continuous current 200A pulse (100uS) 150A pulse (1mS) Low RDSon Low input…
Part Number: CSD18542KTT Hello team,
I have a question.
What conditions did you use to measure RθJC? I don't know what kind of substrate and heat sink you used like other FETs, so please let me know.
Regards,
Masa
Part Number: CSD18542KTT Other Parts Discussed in Thread: CSD18542KCS , LM25116 , CSD18543Q3A , CSD18534Q5A Hello team,
Regarding following thread,
CSD18542KTT: RθJC
I discussed about thermal resistance with the customer.
The customer is considering…
Naveen,
Sorry, I forgot to look at the schematic again... with a bus voltage of +48V, you CANNOT use this gate driver with a PMOS here. I would suggest using a NMOS MOSFET. NMOS MOSFETS switch faster and have less R_DS On than PMOS as well (as a general…
Part Number: CSD18542KTT Hello, I have a basic question concerning junction temperature on my fet and also concerning duty cycle.
I plan to use CSD18542 on the power block for a 3Phase motor. The motor draws current in the order of 1.4A for about 50ms…
Part Number: LM25149-Q1 Other Parts Discussed in Thread: CSD19502Q5B , CSD19505KTT , CSD18563Q5A , CSD18542KTT , CSD18534KCS , CSD17579Q5A , CSD17505Q5A , CSD16342Q5A , CSD15380F3 I've got a LM25149-Q1 design that simulates using the generic Pspice MOSFET models…
Part Number: CSD18542KTT Dear SIr
Does TI have this kind of document as below link??
Due to we meet MOSFET turn-on and gate have ringing issue when I used CSD18542KTT with TI Battery AFE
But in the same layout ,another solution SG60N04G doesn't have…
Part Number: CSD18542KTT Hi Expert,
Most MOSFET TI, ST, On-Semi etc...only give positive Id for N-MOSFET, and negative Id for P-MOSFET.
e.g TI device CSD18542KTT has continuous Id with +200A.
However, Rohm MOSFET always gives both positive and negative…
Part Number: CSD18540Q5B Other Parts Discussed in Thread: CSD18542KTT Hi,
We got a question from the customer about CSD18540Q5B. Could you help us?
[Question] They compared Rds(on) and Qg between CSD18540Q5B and CSD18542KTT. They assume CSD18540Q5B is used…
We are using the CSD19532KTT on the DRV8350RS design and on the CSD18542KTT DRV8320RS design. If I look at figure 8 of the CSD18542KTT there is a difference of .9-1.5x difference between 0 and 100c which the fets could experience between startup and running…