Part Number: CSD19502Q5B Hi Team,
CSD19502Q5B VGS=10V, ID=50A Drain-source on-state resistance can under 3mΩ?
Infineon-BSC030N08NS5-DataSheet-v02_04-EN.pdf
Part Number: CSD19502Q5B Hi Team,
In one of our designs, we use a MOSFET CD19502Q5B. We couldn't find any information about the maximum current of the body diode in the datasheet. It would be extremely helpful if you could share the necessary information…
Hi David,
I have tried:-
Maximum step size = 20ns (and larger/smaller values)
RELTOL, VINTOL, ABSTOL at 10x their default values
Selecting all AutoConverge options (including Restart)
...but I'm still getting these convergence errors:-
I've also…
Part Number: UCC28C40 Other Parts Discussed in Thread: CSD19502Q5B , Dear,
we use UCC28C40 and CSD19502Q5B, power up moments, MOS peak current 8A, and then IC and MOS was demage.
schematic as below chart:
YIAPFJ1907T---- 0531.pdf
If any suggestion, Please…
Sorry, we don't have a better photo, board is defect now. Oszi parameters were 5V/div (0V line is the 2nd line from bottom, so max. voltage is about 18V (=input voltage). And 2µs/div in x-direction (about 100kHz).
We use the gate driver LM 5108…
Hi Nishie,
I would think Q3:CSD17303Q5, Q4:CSD17303Q5 are good choice.
Please reconsider Q1:CSD19502Q5B, Q2:CSD19502Q5B because:
1. Min Vin=5V means the gate driver voltage may be 4.5V, CSD19502Q5B will show much higher Rds(on).
2. Considering 24V max input…
Part Number: LM5175 Other Parts Discussed in Thread: LM5176 , CSD19502Q5B Dear Support, my design has this spec. : Vin=10-32V, Vout=24V, Iout=20A (based on LM5175 or LM5176). My target is to reduce LM517x power loss so I prefer to use Optional input to…