Other Parts Discussed in Thread: CSD19502Q5B , CSD19506KTT We are planning to use High current MOSFET.
Below mentioned our requirement follow this,
1. DC continuous 120A
2.VGS = 9V
3.Low RDSon Example(1mohm to 3mohm)
4.Low input and output capacitance
…
Part Number: CSD19506KTT Other Parts Discussed in Thread: TIDA-00377 , , TINA-TI , TIDA-00751
Dear Team
http://www.ti.com/lit/df/tidrjj8/tidrjj8.pdf
I was trying the TIDA-00377 Solid State Relay SSR using TI TINA 9. I have a custom capacitive load and…
Hello Nison,
Thanks for the inquiry. The CSD19536KTT is our highest performance, 100V FET in D2PAK. The only other option would be the 80V, CSD19506KTT which has slightly lower on resistance (2.3mΩ max vs. 2.4mΩ max at VGS = 10V). However, the CSD19506KTT…
Part Number: DRV8329AEVM Other Parts Discussed in Thread: DRV8329 , CSD19506KTT , UCC27284 , , C2000WARE Hi Team,
The half-bridge gate driver replaces the DRV8329+CSD19506KTT with 3 UCC27284 to control the BLDC and there're 2 issues may need your help:…
Part Number: TPS2491 Other Parts Discussed in Thread: CSD19506KTT Hi,
i would like to have a confirmation from profi. in this field. I'm developing a PCB which needs separate some loads from power supply. The power supply are Super-Capatitors (voltage…
Hi Joshua,
I got the response from customer: I am using the MOSFET CSD19506KTT with Rsense=2mOhm. According to the calculations, IDRIVE=Hi-Z, VDS=Hi-Z . If I set IDRIVE=Hi-Z and VDS=Hi-Z, the driver reports an error and the motor does not rotate at all…
Other Parts Discussed in Thread: CSD , CSD18510KTT , CSD18535KTT , CSD19505KTT , CSD18536KTT , CSD19506KTT , CSD19536KTT , TINA-TI Hi,
I am fairly new to TINA TI, so apologies if I am missing something very obvious.
I am searching for models for the CSD power…
Hi Adam
Needed gate edge rise/fall time? - This is between 80nS to 100nS
FET part number? - CSD19506KTT 80 V N-Channel NexFET™ Power MOSFET
Share Schematic if possible? - PDF attached
Gate and SHx node trace widths? - 8mil PCB trace widths
Distance…
LM5069.xlsx
I have uploaded the LM5069 Calculations. My Input supply ranges from 10V-30V. My OVL:30V and UVL:12V. Max Load Current: 8A I have chosen the Vishay SiJ186DP since there aren't any suitable TI mosfets in stock.