Part Number: CSD86360Q5D Hi,
Can you provide min (0C), typical(25C) and max(85C) RDS_on values with a gate drive of 5V? I see that there is a chart but it is kind of hard to get real values off the chart.
Thanks
Part Number: CSD86360Q5D Hi,
I am looking for the unencyrpted model for CSD86360Q5D to import in Tina, is it possible to obtain this?
Thank you!
Regards,
Alberto
Other Parts Discussed in Thread: CSD86360Q5D , CSD95372AQ5M Hi
Our customer would like to get the SOA curve of "Vds and Ids" for CSD86360Q5D and CSD95372AQ5M.
i.e
There is the SOA curve of " temp and current" on the datasheet.
But do you have…
Part Number: TPS650861 Other Parts Discussed in Thread: CSD86360Q5D , CSD87350Q5D , I have a question about the MOSFET power block for Buck 1, 2 and 6.
What is the maximum capacitance that they can drive?
The two power blocks I am looking at are the…
Part Number: CSD87352Q5D Other Parts Discussed in Thread: CSD87353Q5D , CSD86350Q5D , CSD86360Q5D , CSD17312Q5 Hi Team, we would like to confirm the ESD Information of these devices.
CSD87352Q5D CSD87353Q5D CSD86350Q5D CSD86360Q5D CSD17312Q5
Thank…
Other Parts Discussed in Thread: CSD87350Q5D , CSD87588N , CSD87381P , CSD86360Q5D , CSD87355Q5D , BOOSTXL-TPS650861 , TPS650860EVM-116 , TPS650861 Hi
I want to use the TPS65086100RSKT PMIC.
I want to use BUCK3,4,5 for the following (PVIN = 3.3V…
Hi Noor,
I'd like to clarify/update some parameters in the spread sheet.
Here is the schematic. 0.88V 40A 2phase TPS40422.pdf
Customer used it as dual phase configuration.
Q1: for the PSU parameters, should we fill in per phase parameters or…
Other Parts Discussed in Thread: CSD86360Q5D , TPS40140
Hello
I'm looking for a solution with the following specs:
Output : 175 A @ 2 V max
I was looking to use 4-phase sync buck with the Synchronous Buck NexFET™ Power Block,CSD86360Q5D.
I need…