Part Number: CSD95379Q3M Hello,
Below is customer waveform. negative voltage -2.7V is about 13ns. That voltage and timing looks not specified on datasheet just only -7V <10 ns specification. Has any damage concern for this waveform? Thank you.
…
Part Number: CSD95379Q3M Hi,
we want to use this part to drive an inductor that is tied to VCC/2 on its other end. Current needs to flow in both directions. This part seems to be suitable for this when used in forced CCM. As there is no evaluation board…
Part Number: CSD95379Q3M Other Parts Discussed in Thread: SN74LVC2G126 , CSD Hi,
I'm planning to incorporate CSD95379Q3M in a half bridge push pull design (a half bridge on primary side, and output without inductor). This design has intrinsic ZVS…
Part Number: CSD95379Q3M Hi,
We are planning to use CSD95379Q3M in hysteretic buck converter. Our application requires control FET to turn on with the first toggle on PWM pin only. Initially when we start the operation for first time, we suspect that…
Hi Nickelson,
The model CSD95379Q3M file is encrypted and will work only in OrCAD CIS 15.7 and above. Also, as per End User License Agreement (EULA) of LTSPICE, we can not support model development or debug in LTSPICE.
We can provide the device model…
Part Number: CSD95379Q3M Other Parts Discussed in Thread: LP2985 , I'm having some issues with this part not switching on startup. I'm using two of these to form an H bridge for bipolar control of a TEC element.
My setup:
Vdd = 5V, Vin = 3V
Skip#…
Part Number: CSD95378BQ5MC Other Parts Discussed in Thread: TPS40428 , CSD95379Q3M Hi expert team
Customer is using CSD95378 with TPS40428, and VIN range is 4.5V to 14V, we found that CSD95378 will enter UVLO while VIN is about 4.5V.
But we can't…
Hello,
Most smart Power Stages were designed for multiphase synchronous Buck application.
For 25A/30A Boost converter you can use CSD96370Q5M or CSD96371Q5M.
For 12/15A Boost converter you can use CSD95379Q3M or CSD95377Q4M.
Best regards,
…