That means Main domain (CPSW9G) signal CLKOUT (pin AA25 / AJ28 /Y29) or WKUP/mcu domain signal MCU_CLK_OUT0 (pin H27) both used the sync TDA4 RMII and PHY RMII REF CLK.
Question:
1. How about the CLKOUT driver strength, does it can driver 3 PHY and route…
Part Number: TPS6521815 Other Parts Discussed in Thread: TPS65218D0 , TPS51206 , TPS65218 , TPS51200 Hello,
Hope you are doing well,
We are using TPS6521815 PMIC for powering Cyclone V GX with DDR3 memory, having few queries with sequencing and configuration…
Part Number: TMS320C6655
Hello,
In our current setup we are booting TMS320C6655 without IBL, we are flashing code into the NOR flash memory(MT25QU128) with help of NOR-Writer utility which perfectly working fine.
ref - https://e2e.ti.com/support/processors…
Hi Jake,
May I ask if the Bluetooth module/chip has a certificate or compliance statement that complies with the Radio Equipment Directive (RED) (2014/53/EU)? Or is there a report that complies with EN 300 328, EN 301 489-1, EN 62479/EN 50566?
The summary…
Hi Zack, it looks that the offset override helps us. I try it with Smart RF studio, and it is working as expected.
It doesn't matter if we are working with the 868MHz or with 433MHz on the beginning.
As for the output power I try to update the configuration…
This graph shows the output power vs Fout for 3 different out_pwr indexes.
I am looking for the accuracy of the output power at a fixed frequency and fixed out_pwr index.
For example: At about 3200Mhz and out_pwr index=31 in the graph, it shows about…
How are you handling the /LDAC function? It looks like you can drive the output(s) by:
1) Wiggling the /LDAC pin (after writing the code register(s)) [Ref data sheet (Rev 4) p. 12]
2) Using the LDAC command over the SPI [Ref Table 1]
3) Using the Writethrough…
1) Yes, this appears to be the correct setting [per timer_a.h]:
> #define TIMER_A_CLOCKSOURCE_EXTERNAL_TXCLK TASSEL__TACLK
I don't think you need to change anything else (but try it and see).
2) TA1CLK is available on P1.6 (pin 6 on the PT/RHA packages…
Christoph,
Christoph Spielmann said: When I mention "custom hardware" I am talking about our custom board.
Thanks for the clarification; I suspected you were using half LaunchPad for debugging but it is good to be 100% sure.
Christoph Spielmann…