I'm a bit confused ... in this thread:
https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/933728/dac7718-offset-and-power-on-reset-issue
... Akhilesh K asks David Park (thread starter) to validate the proper…
Part Number: ADS8332 Hi,
Below is the code I am using to test the SPI communication between Arduino Mega 2560 v3 and ADS 8332.
For starters, I am just trying to read the CFR to establish communication.
I am getting '0' as serial output for "Serial.println…
Part Number: AM3359 Hii Sir,
I want to read and write part no and serial no. from SPI flash memory(w25q64)and I am accessing SPI0.
I have one doubt,can I try with test application(spidev_test.c) to read part no and serial no?
I built DTS file for this…
Thanks sir,
I am working on SPI flash memory(w25q64) and I build DTS file for this through SDK and I want to load dts file into board through linux commad . Any command for this?
we can load file through another way but they will take more time.
Here I…
Part Number: PROCESSOR-SDK-AM335X
Hii all,
I am working on SPI flash memory(w25q64).and I am accessing spi0. Here i am putting my dts file.
/*
* Copyright (C) 2012 Texas Instruments Incorporated - http://www.ti.com/
*
* This program is free software;…
Part Number: PROCESSOR-SDK-AM335X
Hii sir,
I am using sdk v04.00.00.04 and AM335x EVM processor.
I want to read and write part no and serial no. for SPI FLASH.
I built dts file for spi flash memory (w25q64) but I don't know what is the next step after…
Part Number: AM3358
hello we have developed an am3358 based custom board with ref design of starter kit
in starter kit there is 4.3 inch touch screen available on board
in our board we are using 7 inch innolux lcd
after successful board boot i am unable…
Part Number: AM3358
hello,
we have developed am3358 based custom dev. board with ref. design of AM335x Starter Kit. in AM335x Starter Kit there is only one DDR3 ram available on board (i.e. MT41J128M16JT-125) but in our custom board there is two RAM (i…
hi Andreas Dannenberg
thank you so much for your interest with this matter
and sorry for UN-sufficient information in question
right now i am working in ti AM335x Starter Kit and using ti latest sdk 6
i want to understand the file execution sequence…
Part Number: AM3358 hello,
we have developed and am3358 based custom board with ref. design of starter kit
in our custom board we have added 4gb eMMC on board
in old ti sdk after modification in
common board filed and other board specific file we are…