Part Number: DAC081S101 I have a SOT-23 package of DAC081S101.
I am connecting this to imx processor via SPI2 interface. SPI drivers are enabled in the processor. SPI loopback test is successful. Connections are as described :
DAC081S101 pins
imx Processor…
Part Number: DAC081S101 Other Parts Discussed in Thread: DAC43401 Hi team,
Could you help recommend the successor of DAC081S101CIMK? P2P is preferred.
Thank you!
Marc
Part Number: DAC081S101 Other Parts Discussed in Thread: ADS7866 , AMC7891 Hi Team, I have customer inquiry below: The customer wants to use an 8 Bit ADC with SPI output to directly connect to an 8 BIT DAC with SPI input to form what will essentially be an…
Other Parts Discussed in Thread: DAC5311 , DAC081S101 Fellows,
My aim is to control a DAC 0-5V analog output, from a 5V supply rail. The SPI bus is controlled by a TM4C12x, which sends logic signals at 3.3V.
I had initially selected DAC5311, and got frustrated…
Other Parts Discussed in Thread: DAC5311 Both are rail-to-rail 8-bit parts with SPI interface. Same price, spec differences are minimal.
Makes you wonder whether they'll EOL one of them. Digi-key has more DAC5311's if that's any indication.…
Part Number: DAC081C081 Other Parts Discussed in Thread: DAC081S101 Hi Sir
May DAC081C081 can support I2C in and output 25KHz square waveform output?.
Bogey
Part Number: DAC0832 Hi Sir,
DAC0832 will be discontinued by 2020. which one would be used as a P2P replacement for it. the page with DAC0832 suggests DAC081S101,but it is not P2P.
Would you pls give some recommendation on it.
Thanks a lot.
Part Number: TPL1401 Other Parts Discussed in Thread: DAC43401 ,
There are many low-cost, 8-bit DACs in TI’s portfolio, but if I only need to create a simple DC bias – what is the lowest-cost solution?