Part Number: DAC104S085 Other Parts Discussed in Thread: DAC60004 , DAC60504 , DAC70504 , DAC7716 Looking a replacement to LTC2634, a quad 12bit with FSO above 2.04V (preferred closed to 5V) ,similr to DAC104S085, but with DAISY CHAIN OPERATION!!!!
Part Number: DAC104S085 Hi,
I'd like to confirm DAC104S085 about power on reset. Then, according to the datasheet Figure 38, the output is about 500mV at VIN≒1.8V. Could the output be always 0V during power up?
Best Regards,
Toshiyuki
Part Number: DAC104S085 I am using a DAC104S085 in a product design. On our initial hardware, I am only able to get the DAC to accept a single command and it ignores any command given after that.
I have tried a variety of commands.
With a single DAC I…
Other Parts Discussed in Thread: DAC104S085 Hi I have a question about D1 and D1 of the INPUT SHIFT REGISTER. Could you plese answer my question?
What are D1 and D1 of the INPUT SHIFT REGISTER? Resolution is 10 bits. I think the bis for resolution is…
Other Parts Discussed in Thread: DAC104S085 Hi,
my customer is going to conduct these two abnormal applied voltage test with DAC104S085
described in attached file. DAC104S085 must work normally after the test.
Can DAC104S085 accept these two test?
If not…
Other Parts Discussed in Thread: DAC104S085 Hi,
I'd like to estimate the total error of DAC104S085 under the conditions.
VA=5V , TA=-30 to +70 degrees C.
I found the application note below in MAXIM's website and try to calculate the total error of …
Other Parts Discussed in Thread: DAC104S085 Hi Team,
Please let me ask about the Start point of Output Voltage Settling Time (ts) of DAC104S085. I found that the specification of ts in electrical characteristics however I could not find the description of…
Part Number: AM3357 Other Parts Discussed in Thread: DAC104S085 , SYSBIOS Hello.
I'm trying to develop devicetree for custom AM3357 based board.
I've encountered strange problem, any device driver declared as 5th child of SPI1, is not able to communicate…
Also note, that errors coming from MCP23xxx and PCF85xxx appear because that chips are not presents on board that I am using and are still defined in device tree.
As a side note, I successfully launched on the same PCB TI DAC104S085 and it works fine…
Part Number: TLV5604 Other Parts Discussed in Thread: DAC104S085 Hi, I was wondering if there is an extended temperature range version of TLV5604IPW DAC?
Thank you,