Part Number: DAC121S101QML-SP Other Parts Discussed in Thread: LMP7704-SP Hello, for a current design we are using the DAC121S101QML-SP. Now we need to provide an output current of up to 20mA. The signal is then transmitted via a harness of 1m. At the sensor…
Part Number: DAC121S101QML-SP Hello,
I had some questions on the DAC121S101QML-SP Gain Error.
Do you have any estimate of the error of the DAC121S101QML-SP Gain Error at End of Life (aka ageing effects, is it an extra +/- 0.1%FSR over life, +/- 1%FSR…
Part Number: DAC121S101QML-SP Other Parts Discussed in Thread: DAC121S101 Hi,
I wanted to simulate a circuit using the DAC121S101 device.
Would you happen to have an IBIS model for this part?
Thanks!
Part Number: DAC121S101QML-SP Other Parts Discussed in Thread: DAC121S101 Hi,
I was wondering if you had information on rise and fall times of the DAC121S101 digital interface, particularly of SCLK.
I did not see any mention of this in the datasheet. …
Part Number: DAC121S101QML-SP Hi,
Can the 5962R07726, space rated version, share the clock(SCLK) and/or data(Din) lines for multiple devices? If so, what is the recommended number devices that can share the data and/or clock lines?
If the data and clock…
Part Number: DAC121S101QML-SP Hello,
For the 5962R0722602VZA (DAC121S101WGRLV), i was wondering whether the package contains floating Metal and if the lid of the device is grounded. Thanks!
Best,
Adam
Part Number: DAC121S101QML-SP Other Parts Discussed in Thread: MKT-WG10A-MS Hi Team,
Can you please support with dummy packages of following devices?
List of ICs used
Package
DAC121S101WGRQV
NAC0010
Thanks in advance
Best Regards
Furkan…
Part Number: DAC121S101QML-SP According to the datasheet:
"7.3.4 Power-On Reset The power-on reset circuit controls the output voltage during power-up. Upon application of power, the DAC register is filled with zeros and the output voltage is 0 V and…