Part Number: DAC38RF82EVM Hi,
I am looking for a sample FPGA project using DAC38RF82EVM + iwave iW-RainboW-G30D (Zynq Ultrascale+ MPSoC (ZU4) SOM)
Thanks, Divya.
Part Number: DAC38RF82EVM Other Parts Discussed in Thread: DAC38RF82 , Hello,
I am evaluating DAC38RF82 with the evaluation board (DAC38RF82EVM) and the TSW14J57 pattern generator with high data rate.
A 1100 MHz / +6dBm signal is fed to the input of the…
Part Number: DAC38RF82EVM Other Parts Discussed in Thread: DAC38RF82 Hello,
I am evaluating DAC38RF82 with the evaluation board and the pattern generator.
A 100 MHz / +6dBm signal is fed to the input of the LMK (J4 connector).
With the following configuration…
Part Number: DAC38RF82EVM Other Parts Discussed in Thread: DAC38RF82 , DAC38RF82 The SYNC signal is high when it is powered on I encountered a problem when debugging the DAC38RF82, as soon as the chip was powered on, it remained high without JESD204B link…
Part Number: DAC38RF82EVM I encountered difficulties in using DAC38RF8xEVM. After the JESD204b link was established, SYNC kept toggling, and DAC had no signal output.
Clock circuit adopts On-Board VCXO Clock Mode (CMODE4) in DAC38RF8xEVM to change the…
Hi,
Sorry for the long delay. Attached is configuration file which achieves 6144MSPS, Dual DAC real input, 4x interpolation, and accepts a 10MHz reference into J4. Ensure that JP10 is removed and that JP3 is connected. After loading this configuration…
Part Number: DAC38RF82EVM Other Parts Discussed in Thread: DAC38RF82 , , LMK04828 , LMK04832 Hello,
I am evaluating DAC38RF82 with the evaluation board (DAC38RF82EVM) and the TSW14J57 pattern generator.
A 100 MHz / +6dBm signal is fed to the input of the…
Part Number: DAC38RF82EVM Other Parts Discussed in Thread: DAC38RF82 , TSW14J57EVM Hello, I am begining evaluation of DAC38RF82 chip using DAC38RF8xEVM evaluation board with TSW14J57EVM pattern generator.
I followed the DAC38RF8xEVM User Guide in order to…