Part Number: DAC38RF89 I need to get the Eye Scan GUI software for testing a DAC38RF89, the SLAA762 says how to run the test but says we have to request the software on E2E. I found a link under this post https://e2e.ti.com/support/data-converters-group…
Part Number: DAC38RF89 Other Parts Discussed in Thread: DAC38RF93 Hello,
I ran into a problem recently with trying to run HSDC Pro to troubleshoot a suspected JESD problem with our DAC38RF89 implementation. I installed from the website, but get a "Missing…
Part Number: DAC38RF89 Hello,
We are using the DAC38RF89 and we encountered a problem at -20 deg temperature.
The output transmits 200M to 4G at full scale power.
The power delta at 25 deg is about 6dB for this frequency bandwidth, between the power…
Part Number: DAC38RF89 Hi Team,
The customer use a self-study board to develop LMFs=8212 for DAC38RF89 with the following configuration:
The JESD204B design on the FPGA side is as follows:
When DDS-IP on the FPGA side is enabled to send to the…
Part Number: DAC38RF89 Other Parts Discussed in Thread: LMK04828 The DAC output is 1100MHz. There are spurious of 1M and 37.5M, respectively.
The PLL configuration of the DAC is as follows:0x31 0x0400; 0x32 0x0508;0x33 0x2A24.
The DAC clock is 200MHz of…
Part Number: DAC38RF89
Hello,
I'm Using the DAC38RF89I and wanted to know what is the best way to place the BALUN peripherals.
For mechanical issues I can't use parts in the Print side (P.S) with thickness bigger then 0.3mm, so the inductors could…
Part Number: DAC38RF89
Hello,
Some questions regarding the DAC38RF89 Currents:
1. In Figure 149 (Power Supply Scheme) The VDDDIG1 Current shown is 2.5A ;
While in the "Electrical Characteristics - DC Specifications" (Section 7.5) The Max Current…
Part Number: DAC38RF89 Hi, Our customer have two questions.
1 Is there a spec for the output jitter of the internal PLL (including VCO)? Also, is there a way to calculate jitter?
2. If we set the same data for two outputs and start sending, Will there…
Part Number: DAC38RF89 When debugging, everything works well when 204B interface channel rate is 10G. When a t 12G, the SYNC signal is occasionally pulled low, causing resynchronization.
The other registers are unchanged, except for the corresponding modification…