Part Number: DAC5672EVM
Hello,
my customer is looking for the DAC5672EVM PCB Files in Altium format. He wants to design a PCB, that connect with the DAC5672EVM; so he needs more information about this the EVM, such as the Size and the fixed point size…
Part Number: DAC5652AEVM Other Parts Discussed in Thread: DAC5672EVM Hi,
I have the following configuration:
1) Zed board connected as data source; output = 1MHz 14-bit sine output.
2) TCXO generating 40MHz LVCMOS output as clock reference.
3) DAC5672EVM…
Part Number: TRF3703-33EVM Other Parts Discussed in Thread: DAC5672EVM , DAC5688 , DAC5688EVM We have been working with the TRF3703-33 part and are wondering if there is a development board that has the below with an FPGA for the data_in interface?
I did…
Hi Allen,
Welcome to E2E. I apologize for the delay in this response.
TI does offer EVM solutions that would handle this, but not at the scale you are looking for. A few examples would be the DAC5652AEVM or the DAC5672EVM . If you prefer to look at all…
Taketo,
If the FPGA's mentioned in this post have the same data sheet specs as the Altera EP4SGX70HF35C3N FPGA, they should work just fine. This is the FPGA used by the TSW1400EVM which works with the DAC5672EVM up to 275Msps data rates. Other considerations…
Satoshi,
There is no EVM for this device. The customer could purchase a DAC5672EVM and swap out the DAC5672 with a DAC2904 as they are pin for pin compatible. Or they can evaluate the DAC5672A, which has better performance.
Regards,
Jim
Hi Andrew,
From the screen shot it seems like customer is only toggling WRTA once where as CLKA is toggled 4 times. These two always should match as the WRT is used to latch the data in before it goes to the DAC.
Also looking at the Iout it seems like…
Other Parts Discussed in Thread: DAC5672EVM , ADS4226 , ADS4226EVM , ADS62P24 , ADS62P29 I'm a newbie to this field and even do not have a FPGA board yet.
I'd like to calculate the budget beforehand and decide the components for new FPGA implementation…