Part Number: DAC60508 Hi!
I will use DAC60508.
I plan to connect a 1m lead from DAC60508 on the circuit board to the data logger.
The document of DAC60508 says 2kΩ and 10nF load to GND is possible,
so is this case OK?
Part Number: DAC70508EVM Hi Experts,
Our customer is evaluating DAC70508 EVM, and found a strange issue when VDD/VIO used the same 3.3V power supply, it can not change REF DIV and Output Gain registers correctly, but if used the separated voltage like…
Part Number: DAC70508 I believe I've configured my device correctly however I must have made a mistake since the output voltage out of my DAC's is only 0-1.25V instead of 0-5V. I'm using a voltage to CODE conversion factor of 3276.6 (Vout = CODE…
Part Number: DAC3174 Dears,
Could you help to review the two schematic, thanks!
two DAC are synchronized;
Output ±5V single-ended signal;
100MSPS
DAC3174 synchronization.pdf
DAC70508 output.pdf
Part Number: DAC80508 Other Parts Discussed in Thread: DAC70508 Hello all!
I am having a little trouble setting the output of the DAC70508 DAC.
I think i have everything set up correctly as far as MSB, LSB etc... The CS line and SPI is looking good on…
Hi Dragan,
DAC70508 , 14 bit, 8 channel - noise density 50nV/rHz @ 1kHz G=1 and internal reference
DAC70004, 14 bit , 4 channel - noise density 60nv/rHz @ 1kHz, and external reference.
TI had recently released very low noise device DACx1001 family with…
Part Number: DAC7568 Other Parts Discussed in Thread: DAC70508 , DAC80508 Dears,
Is there any sample code for DAC7568?
My customer needs it to help their design speed.
Thanks.
Part Number: DAC80501 I am using the DAC80501 with the internal reference and a 3.3V supply. My I2C communication works correctly but I am unable to update the DAC output. What is going wrong?
Part Number: DAC80508 I would like to implement communication with the DAC80508 on my microcontroller, do you have any examples that will help me get started?
Part Number: DAC60508 Hello,
I'll likely be using a DAC60508 in an upcoming project and while browsing the datasheet I came upon the following quirk (?):
page 22: 8.3.1.2 Output Amplifiers: Table 1 says that setting both DIV and GAIN to 1 is "Not…