Part Number: DAC7562 Other Parts Discussed in Thread: DAC63204-Q1 , DAC63202 , DAC63204 Hi team,
A customer is looking into the DAC7562, they would like to have a newer DAC the following requirements:
Fully protected DAC output for automotive environment…
Hi Katlynne-san,
Katlynne Jones said: I should have the test results by Monday to verify the commands needed to update DAC A & B at the same time.
->Thank you for your support.
I look forward to the test results.
Katlynne Jones said: Are you asking…
Part Number: DAC7562 Hi,
Regarding the soldering of DAC7562SDGST, is there any problem referring to the following materials? Or is there any material about soldering for VSSOP package?
https://www.ti.com/jp/lit/an/spraby1a/spraby1a.pdf
Best Regards,
…
Part Number: DAC7562
Hi,
Which of the following commands should be written when using DAC-A/B with Gain=2 using internal reference?
1) [C2:C0]=111, [DB]=1 (8.4.4 Internal Reference Enable Register)
2) [C2:C0]=000, [A2:A0]=010, [DB1:DB0]=00 (8.4.2 Gain…
Part Number: DAC7562 Hi,
Is it correct to assume that the DAC operation by HW reset using CRL pins (Register value, Vout output value, etc.) and the DAC operation by SW reset (DB=0) are the same?
Best Regards,
Nishie
Part Number: DAC7562 Hi team,
Can we use DAC7562 with keeping CLR pin at High for all time?
Or do we have to change from L to H when starting?
Best regards,
Kento
Part Number: DAC7562 Other Parts Discussed in Thread: LP2985
Dear Team,
I am using DAC7562 with an external refrence.Below is the schematic.
May I know is this fine or not.
Do I need to take care anything particular in Hardware or Firmware when I am…
Part Number: DAC7562 Other Parts Discussed in Thread: OPA140 , LMH6503 , TINA-TI
Hi,
An application question for the DAC7562 12-bit version.
Any suggestions for the datasheet bipolar output circuit (page 44) to work with +/-5V supplies and output -/+1V…