Part Number: DAC7728 Other Parts Discussed in Thread: TMS320F28379D , Dear Sir,
I wanted to use DAC7728 with the controller. I need to know that the timing requirement of the DAC is compatible with TMS320F28379D or not ?
Do I need more components to meet…
Part Number: DAC7728 Will the DAC7728 work properly if it is not brought up in the sequence outlined in the datasheet? I am having a problem with being able to sequence the AVss rail as it automatically comes on. The datasheet says the digital initialization…
Part Number: DAC7728 I am able to write to a single DAC channel and get the output I want, and I am able to read back the value written to the register. When I try and write to the next DAC after that I get no response from it and the output voltage doesn…
Part Number: DAC7728 Hallo,
I need some help with the DAC7728.
I need to simulate different voltage levels in an isolated environment (via opto-couplers). The power supply is also made potential-free. I try to program the DAC in following steps:
- R/W…
Part Number: DAC7728 After completing our Alpha design, and 10 units, we found the DAC range we need is much less than anticipated. However the precision we need is higher. We are using a 1.024V reference with a 4x multiplier. So our DAC output is 0-…
Part Number: DAC7728 Hello, I have design a pcb board, which 2 DAC7728, my configuration:unipolar output, i don't use the correction engine, 15V for AVDD, IOVDD is connected to DVDD and is 5V, i dont use LDAC Some time one is not starting (all time…
Other Parts Discussed in Thread: DAC7728 , OPA2277 Hello,
I made a board with a DAC7728, used in bipolar mode (±15V). Vref is 2,5V, gain is set to 4x.
But some of this chips is fired in some PCB boards. I found the fired line is ±15V. So, I am afraid…
Other Parts Discussed in Thread: DAC7728 Hello , I am working with a DAC7728 interfaced to the DSP F28335 . I configured the XINTF with the maximum number of cycles for reading and writing , but I can not correctly read the contents of the registers of t…