Part Number: DAC80501EVM I'm using a Teensy 4.1 to control this eval board through SPI. JP1 and JP2 closed, JP3 and JP4 open. Even if the ref div is set to 1, I still cannot get DAC output. I also cannot shut down the internal reference. I used the same…
Part Number: DAC80501EVM Hello,
I installed DAC80501EVM and USB2ANY with Lab view Run Time Engine 2014
It is impossible to modify VOUT. VOUT is always = 0.0000V
How is it possible to set up DAC80501? Can you please help me.
Best regards,
Thierry.
Part Number: DAC80501EVM I am running DAC80501EVM in SPI mode with wires connected to my main board. (VDD 3.3V, VREF 2.5 Externally connected with REF_DIV and GAIN_MUL set to 1 each)
I am running all operations as normal until I change operating mode…
Part Number: DAC80501EVM Hi Team, Just for verification. What exact variant of DAC80501 is integrated within the DAC80501EVM? Is it the Z or M variant? Kind Regards, Jejomar
Part Number: DAC80501EVM Hello guys,
One of my customers is trying to evaluate DAC80501 using DAC80501 EVM with USB2ANY.
DAC80501 EVM
http://www.tij.co.jp/jp/lit/ug/slau795/slau795.pdf
At this moment, the EVM control software on their PC is not operated…
Part Number: DAC80501EVM
Tool/software: TI C/C++ Compiler
Hi,
I am trying to use the DAC80501EVM with the USB2ANY along the software GUI provided by TI.
The software shows that the device is connected but there is no change in response at vout.
The GUI…
Katlynne,
Thanks for the quick response --
I also don't have the DAC80501EVM installed, I was just going by the manual (section 3.2.2.1 Low Level Configuration Page).
I would suggest that TI clarify (and clean up) the data sheets on the DACx70501…
Part Number: DAC80501 Hello, I've been reading carefully the DAC80501 datasheet and it's not clear how to read the registers in SPI mode. Writing to the registers is well explained but reading them is not clear. Can you clarifiy if is it possible to read…
Hi Paul
Below is Help text for people who purchased totally fatal and not checked DAC80508EVM board and have Win'10 64 bit in use.
1) Do NOT install LabView NI RTE 2015 or another. Only LabView NI RTE 32 bit 2014 is OK and should be installed.
…