Part Number: DAC80508 Hello, I would like to have more specific information about the TUE. I noticed regarding the DAC80508 component that the TUE reported on the datasheet has typical values of 0.05% and maximum values of 0.1%FSR. I found on some documents…
Part Number: DAC80508 Hello everyone,
I would like to know the TUE of the DAC80508 using the internal reference, a gain of 2, and a divider of 1.
Thank you
Luigi
Part Number: DAC80508 Other Parts Discussed in Thread: REF6225 , DAC128S085 The exact device I have is DAC80508ZRTER. That is, ZERO/SDO version.
Three questions:
1. What exactly does "Not recommended" means in the Table 1 for the "1/1" Div/GAIN setting…
Part Number: DAC80508 Question about the datasheet:
The WDFN land pattern shows 0.8mm center pad.
However the Figure 80, QFN Layout Example, shows a large center pad with 5 vias fitted into it. Is it recommended to put extra copper around the pad, and…
Part Number: DAC80508 Hello team,
We need your help to solve a trouble for getting the output on the device.
We're in trouble as listed below.
- When wriiing 0x7FFF to DAC0-DAC7 on register, the output level remains at 0V.
- There is no change in the…
Part Number: DAC80508 Dear friend,
My customer test the chip REF directly which just set the CS low and high. The register setting is default and used the internal reference.
They placed 1uF capacitor between REF and GND.
Here is CS low. Ref voltage is…
Part Number: DAC80508 Hello,
I am a bit confused about calculating the total noise from the DAC Outputs. Specifically I don't understand this table
(Can be found on page 8 of the datasheet)
I think it is first telling the noise over the bandwidth…
Part Number: DAC80508EVM The 80508EVM is connected to USB2ANY.
USB2ANY Explore works ( I done update with USB2ANY hardware ) .
Next, I run the DAC80508 Software. It is in demo mode. I try initialize, but it fails.
Please, give me advice.
Other Parts Discussed in Thread: USB2ANY , DAC80508 Good morning
I am trying to use the USB2ANY with the DAC80508EVB.
When starting with the DAC80508 software the 3V is not available. I think it is needed by the EVB
If I start the USB2ANY utility I can…