Part Number: DAC80508 Hi Sir,
I have some technical queries on DIV, GAIN value for DAC80508MC.
My design spec) 16bitDAC : I use DAC80508MC. 1) 0V output when Reset 2) Data write ± Output 10V.
Investigation)
For the configuration of figure 78…
Part Number: DAC80508 Hello E2E,
I'm studying the Digital feedthrough and Code change glitch of DAC.
They are all specified as the area of the impulse in " nV-sec ".
Take DAC80508 as an example, its performance is as follow.
Is the 4nV-s…
Part Number: DAC80508 Other Parts Discussed in Thread: REF6225 Originally asked in this thread: https://e2e.ti.com/support/data-converters/f/73/t/836424
Moving this question to a new thread
Andrzej asked: "
How to connect external reference voltage…
Part Number: DAC80508 In the datasheet for the part, there are two images of the exposed thermal pad.
4205254
4206446
Which one is correct for DAC80508ZRTET ?
Part Number: DAC80508 Hello!
I want to buy a DAC. The condition is that it can output millivolt level voltage, such as 4MV, and the frequency is 100Hz. Is there a suitable DAC recommended?
At present, I have a dac80508 evaluation board, but I found…
Part Number: DAC80508 Hello! I am using dac80508evm to connect my microcontroller, i.e. CS, SCLK, SDO, SDI, GDN and vio (3.3V), with external VDD of 5V.
At present, I have written the SPI program about microcontroller. I want to start with reading device…
Part Number: DAC80508 What is the default (reset) value for REFDIV-EN (the reference divider). On page 34, Table 13, it is listed as 0/1. Is it 0 for the Z devices and 1 for the M devices?
Part Number: DAC80508 Other Parts Discussed in Thread: SN74ACT244 Hi team, I am using DAC80508 to generate a sine wave. But I've another device SN74ACT244 working in parallel with the DAC to generate a sine wave. The SN74ACT244 SN74ACT244 will be driven…
Part Number: DAC80508 Other Parts Discussed in Thread: USB2ANY
I have attached an image of the evaluation module software for the DAC80508 connected via USB2ANY. I have plugged in the 8 DAC outputs to observe their behavior but I am not seeing anything…
Part Number: DAC80508 Hello,
I see in the DAC80508 datasheet that the SCLK speed is limited during SPI read transactions. Those frequencies are details in Table 7 of the datasheet.
Is the limitation of the read speed due to the SDO output…