Part Number: DAC80516 Other Parts Discussed in Thread: ISO6763 , ISO6760 , ISO6462 i am designing using DAC80516. i need to isolate each channels of the DAC Output. What would be the best way to do that?
Should i isolate the spi signals right before…
Part Number: DAC80516 I am encountering an issue where bit 3 of RESET_FLAGS (AVDD_COLLAPSE_FLAG) is always set on my DAC80516. The DAC performs normally, with percise outputs and cuccessful chip_id reads - but this flag won't go away after being cleared…
Part Number: DAC80516EVM Hi everyone,
I am using the DAC80516EVM with an external microcontroller over SPI.
I have successfully communicated with the DAC using a 5 V microcontroller with the default EVM jumper configuration , and everything works…
Part Number: DAC80516 Other Parts Discussed in Thread: DAC80502 , , DAC80508 , ADS8688 , ADS9324 , AMC7924 Hello guys, I am currently working on a device with 18 cells. I need a DAC for each cells and I was wondering if you had a DAC of 16 channels that…
Part Number: DAC80516 Other Parts Discussed in Thread: DAC80508 , DAC81416 , Tool/software: hi sir
we need a solution, which 16bit/16ch with Daisy chain
did you have the solution?
thanks
Part Number: DAC80516 Tool/software: Hi,
Do we have any suitable device to compete with AD45535(ADI)?
Another question is in what scenario need 200V output amplifier?
Thank you,
Yishan Chen
Part Number: DAC80516 Tool/software: Hi team,
1. May I know the DAC output value before powering up?
2. May I know the DAC output value when powering up the device(AVDD or VIO is below the recommended minimum operating value(by at least 200mV))? …
Part Number: DAC80516 Tool/software: Hi team,
May I know the pin connection of pin below when the customer doesn't use this pin?
1. LDAC: NC(No connection)? GND?
Best regards,
Shunsuke Yamamoto
Part Number: DAC80516 Other Parts Discussed in Thread: DAC81416 Tool/software: Hello,
I have an application where we need a DAC with 12 channels of 16 bit accuracy. For efficiency we want to write all the outputs in one SPI transaction. The part DAC81416…