Part Number: DAC8218 Other Parts Discussed in Thread: DAC8718 , , DAC7718 Because of the supply chain issue with the DAC8718, we plan to use the DAC8218.
The DAC is only used to test ADCs in our Controller Board (so the resolution of 14-bit or 12-bit is…
Part Number: DAC8218 Other Parts Discussed in Thread: DAC81408 , DAC71408 Hello,
I need to generate several analog output signals with voltage range -0.5V/+28V. DAC8218 seems the only available option, but what is written at page 39 of the datasheet about…
Part Number: DAC8218 Hi team,
My customer connect the cap and resistor in the output of the DAC8218.
But if the cap is about nF, the output has long rising edge and 100kHz ripple and the overshoot.
1. So does the nF cap is too large for the DAC8218…
Part Number: DAC8218 Hello Team,
My customer use our DAC8218, you can find the test waveform below, when CLR pin changes from low to high, we can find output has a big spur, the max voltage is about 3V, and last about ~us. Can you help to explain why…
Part Number: DAC8218 Dear all
I have a confusion about some parameters of DAC8218's digital IOs.
1. As for the GPIOn, in absolute ratings, it shows maximum current is 5mA. I want to know whether this is maximum output current or input current, or…
Part Number: DAC8218 Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models Dear all
I find that DAC8218 has IBIS model, I have transferred IBIS model to pspice library, but I'm not very sure how to use this model. It only has…
Other Parts Discussed in Thread: DAC7718 , DAC8718 Hi Eugenio,
please do you have any idea because we have presentation in two weeks, where our analogue outputs should be shown. Shall we check if DAC7718 or DAC8718 is running. Nobody would check 12 bits…
Other Parts Discussed in Thread: DAC8218 , DAC7718 , DAC8718 , REF5040 , DXP , DAC8218EVM , REF5030 Hi,
we have a big problem using a DAC8218. Our communication with the device works well. Which we can see at the GPIO handling. We can write and read the registers…
Other Parts Discussed in Thread: DAC8218 In the data sheet for the DAC8218 (sheet 54- POWER-SUPPLY NOISE), it states that "The 1μF to 10μF capacitors must be the tantalum-bead type". However looking at the evaluation board and BOM, the capacitors…