Part Number: DAC1220 Other Parts Discussed in Thread: DAC8560 , DAC11001A Hi Team,
Hope everything goes well. One customer were facing a problem while using our DAC1220.
Q: when system power up, it will takes 100ms for MCU(F2803x) to wake up. Before…
Part Number: DAC70501 Other Parts Discussed in Thread: DAC8560 Dear Specialists,
My customer is considering DAC70501 for +/-10V output.
They're thinking about using SLAU525 reference design.
The voltage reference of DAC8560 and DAC70501 are slightly…
Part Number: DAC8760 Other Parts Discussed in Thread: DAC8560 , DAC7760 ,
Greetings,
I have a customer using the DAC8760IPWPR, but is facing supply shortages. The customer is actually only using the voltage output from the device. The DAC7760IPWPR…
Hi Kevin,
Does the MMB0 board that comes with DAC8560 compatible with DAC8568?
Because, I see that pin configurations of DAC8560 and DAC8568 are different. If not, what modifications are to be done to MMB0 for it to be compatible with DC8568?
Will…
Hi Akhilesh,
I have been looking into the TIPD design guide that you have suggested me. It is said that for the DAC8560 the choice of Rg2 = 8.25kOhm will result in peak current draw from reference source to be around 333uA, which is under 20mA limit…
Hi Joseph,
I checked the Vrefout and Vrefcom which both of them are 2.5V and they were stable. And about the proper reference input, if I understand your saying, I set the REFSELT[1:0] bits to 10 as it says internal reference selected.
Furthermore…
On further inspection, I was able to capture the activity happening on my MOSI, CLK, and STE pin. My STE and MOSI pins are operating as intended however there is a slight spike at the beginning which concerns me. I also noticed for my clk signal that…
I apologize if I did not clearly describe the problem that I am having. The problem is not with using an external reference for the DAC8560EVM. The problem is that I cannot disable the internal referenve according the write sequence specified on page…
Part Number: BQ27GDK000EVM Other Parts Discussed in Thread: REF3240 , DAC8560 , BQSTUDIO , BQ27530-G1 , INA220 , EV2400 I had an issue with the BQ27GDK000EVM and received the more detailed schematic in PDF form. After probing the test points I found that…
Hello,
I suspect the ADI device is AD5683R. At this time the nearest replacement to this device in the TI portfolio is the DAC8560.
The DAC8411 does use the supply voltage as the reference voltage, but it does not require much current. It is possible…