Part Number: DAC8760EMC-EVM Other Parts Discussed in Thread: DAC8760 Hello,
I have recently received a DAC8760EMC-EVM along with a SM-USB-DIG. I have connected +/-15V supply to the DAC8760 EMV board and also connected the SM-USB-DIG between the USB port…
Matteo,
Here are a few answers for you about the DAC8760:
1. I would tie the HART-IN to GND through the 22nF capacitor to ground.
2. The DAC only supports SPI mode 0.
3. Yes, the LATCH can be tied to /CS. Data is latched in at the rising edge of /CS…
Part Number: DAC8760EMC-EVM I am having one doubt regarding supplies to the board. What must be the current rating of supply for supplying +/- 15V. Can I supply it from a DC Regulated Power Supply of +/-15V, 0.5A rating? Will it damage the board?
Part Number: DAC8760EMC-EVM Other Parts Discussed in Thread: DAC8760 I am working on a project and I need bipolar 10V output for my project. I am thinking of using DAC8760, but couldn't find DAC8760 development board. I came across this evaluation module…
Part Number: DAC8760EMC-EVM
Hello everyone,
I am using the DAC8760EMC-EVM with SM-USB-DIG platform. I send command to DAC using your software. I run the program I made some changes and click on the button Write all Reg, but I noticed that changes are…
Other Parts Discussed in Thread: DAC8760EMC-EVM Hi Sirs,.
What`s differents of DAC8760EMC-EVM version between 2013/2014? customer asks the PCB file for 2014 , is it necessary ?
thanks
Regards,
Philip
Other Parts Discussed in Thread: DAC8760EMC-EVM , DAC8760 I purchased a DAC8760EMC-EVM from Mouser.com (serial number 001 on the silk screen). When +12V is applied to the +15V power connector with the -15V and GND connected to ground, the tantalum capacitors…
Part Number: DAC8750EVM Other Parts Discussed in Thread: DAC8750 , DAC8760 , REF02 , , DAC8760EMC-EVM
Hi,
so bought EVM from mouser, comes with no disk... OK, go to TI website.. not easy to find but eventually found it ( I think) sboc432b.zip
Now, if you…
Dheeraj,
There are two different evaluation boards for the DAC8760. For one, the diodes protect through the full range of supply operation. For that, it is the DAC8760EVM, and you can find the EVM User's guide here:
https://www.ti.com/lit/pdf/sb…