Part Number: DDC1128EVM
Hi guys,
Our company is evaluating the use of the DDC1128EVM. We would like to get the datasheet in PDF format to evaluate the technical features and understand if it is suitable for our needs.
Is it possible to have the datasheet…
Part Number: DDC1128EVM Other Parts Discussed in Thread: DDC112 Hello
I would like to use the dual-channel DDC112EVM to measure two photodiode current signals.
With the photodiodes I measure the absorption of gas in the MIR region of light, where the light…
Part Number: DDC1128EVM Other Parts Discussed in Thread: DDC1128 Hello Guys,
Good day.
Our customer is looking for the dimension and technical information for this evaluation board.
He is building a test system that has 100 channels per board, and there…
Part Number: DDC1128EVM Dear TI technical support, we would like to purchase the optimal wall power supply adapter for the EVM board.
J18 only accepts dc voltage from 7V to 10V. Is there any restriction on the output current or power rating of the ac…
Part Number: DDC1128EVM Other Parts Discussed in Thread: DDC1128 ear TI,
I developed a "Daughter" Interface board for DDC1128EVM for receiving very low DC signal signal from PCBs photodiode sensors.
I use coaxial cable with SMB connectors to…
Part Number: DDC1128EVM Other Parts Discussed in Thread: DDC1128 Dear Experts,
I'm runing the software provided after NDA with Windows 10 64-bit machine. The software has been installed and works apparently well. The program starts and displays windows…
Part Number: DDC1128EVM Hi guys,
So I am trying to write a python code to fetch the data from DDC1128EVM board.
I have made some progress with fecthingthe data but there are some issues in it!
I have 192 buffer full with data not all 256. No idea why…
We don’t provide/disclose/share/support example code for the DDC264EVM.
We had a customer who created some sample code to read from DDC1128 EVM. github.com/.../DDC1128EVMDDC1128EVM uses the same DLL file as DDC264EVM. Though we have not tested the…
Part Number: DDC1128EVM Other Parts Discussed in Thread: DDC1128 Dear Specialists,
My customer is testing DDC11C128EVM and has inqries.
I would be grateful if you could advise.
---
We are proceeding with verification on the evaluation board of DDC 1128…
Part Number: DDC1128EVM Other Parts Discussed in Thread: DDC1128 Hi,
If there more appropriate place to discuss DDC1128 since the EVM is under NDA?
I have a question regarding the voltage reference, not sure if I should post it here
Zulhadi