Part Number: DEM-OPA-SO-1A FOR EVAL BOARD : DEM-OPA-SO-1A, WE REQUIRED BOM TO BE POPULATED ON THE PCB WITH SCHEMATICS, ASSEMBLY INSTRUCTIONS AND TESTING PROCEDURE AS PER DATA SHEET.
Part Number: BUF602 Other Parts Discussed in Thread: DEM-BUF-SOT-1A Dear TI experts,
I'm designing a circuit for the BUF602 based on the schematics in the DEM-BUF-SOT-1A demo fixture ( https://www.ti.com/lit/ug/sbau117a/sbau117a.pdf?ts=1657731211992&ref_url…
Part Number: DEM-OPA-SOT-1A Image of this PCB has no standoff screw holes at four corners but PCB layout in the datasheet shows standoff screw holes. Can you confirm if demo board will have standoff holes?
I am looking for assembly drawing and pick and…
Part Number: DEM-BUF-SO-1A Hi Team,
A customer has this board but they are having 10x attenuated output and not unity gain.
The board was assembled as per the schematic with the corresponding value:
Rin1 = 50 ohms; Rin2 = 25 ohms; Rout 1= 50 ohms; Rout2…
Part Number: DEM-OPA-SOT-1A Other Parts Discussed in Thread: THS4121 Hi team,
My customer would like to use DEM-OPA-SOT-1A EVM boar to evaluate OPA300AIDBVT and OPA657NB/250.
Could you please clarify the package in which feedback resistor and optional capacitor…
Part Number: DEM-OPA-SOT-1A Hi Team, Need your assistance on this minor discrepancy that one of our customer had raised. On the pin configurations pin 5 is /DIS and pin 6 is Vs+. We have noticed that on the DEM-OPA-SOT-1A typical application circuit (Figure…
Hello Prathmesh,
The closest alternative to REG104FA-5/500G3 is TL1963AKTTR, which is offered in TO-263 (KTT) package.
For REG103GA-3.3, the best alternative is TPS7A2633DRVR which is not on the same package, but similar specs. Another option is TLV76133DCYR…
Hi Sankalp,
I would recommend 2 pcs TPS62932 to get Input Vin 15V, output 3.3V(1A) and 5V(0.5A). It is 3.8-30V input, 2-A, 200kHz to 2.2MHz, low-IQ synchronous buck converter in SOT-583 package.
Thanks and kindly let us know anything unclear.
BRs
Luci…
Hi Ranjith,
Thank you for providing that information. We have TLV75201PDSQR as an adjustable dual LDO which each rail can handle up to 1A , and each rail is independently set. This dual LDO is adjustable with high PSRR and comes in a small package:
…