Part Number: CC2650STK Other Parts Discussed in Thread: BLE-STACK , I am trying to get the display / watch to work with the current version of the SensorTag (Seal Date 6/21/17, Rev 1.42). This SensorTag was purchased from Digikey 2 days ago.
I downloaded…
Hello YiKai Chen,
I checked the battery, it is Ok.
I have a solution for my case: CC2650STK is working normally after debugging,
- if I unplug UBS cable --> CC2650STK do not work.
- However, If I remove Devpack Debug --> CC2650STK still works…
Part Number: CC2640
Hi TI Experts,
I met the following issue. Please double check them. [Issue] When I updated the SensorTag firmware for WATCH and LED on latest SensorTag App, the sensortag app did not work correctly. It means that not show the original…
Other Parts Discussed in Thread: CC2650 Hi,
I would like to use the LCD (devpack watch) together with devpack debug on CC2650 sensortag running Contiki 6LoWPAN.
When I started to look through the hardware documentation for all 3 boards I realized that it…
Hi,
I'm using sensortag with display DEVPACK-WATCH and it works fine when it is connected directly on sensorTag but it is rather annoying to unplug debugger, connect display and test firmware each time I modify something. Is there a way to work with…
Other Parts Discussed in Thread: TMP007 , CC2650 Hello TI,
I use the application SensorTagDevPk.eww on IAR Embedded Workbenc h. I have some problems with display sensors data on lcd DevPack Watch. It is possible to display rawTemp or rawObjTemp with dev…
Other Parts Discussed in Thread: CC2650STK Where do I find up to date firmware to run the Watch DevPack for the SensorTag 2.0? Instructions on TI's website show that it should be available in the iOS and Android apps however current SensorTag 2.0 firmware…
Other Parts Discussed in Thread: CC2650STK This is big enough for its own thread: It appears that the latest Debug DevPack XDS110 firmware (version 2.3.0.1) fixes the CC2650STK SPI (external flash / Watch DevPack) conflict with the JTAG interface. I'm…
Other Parts Discussed in Thread: CC2640 I see that there is an example now of the Sharp Display (Watch DevPack) and the SensorTag.
I still fail to get anything other than a few random dots on my display.
I read in the display_readme.txt,
" For SensorTags…
I see references to an example project for the Watch Devpack. I have the BLE 2.1 stack but cannot locate it. Could someone point me to the CCS project?