Part Number: TMS320F280025C I like to display some data from the target device in a GCS graph. I'm using v3 of the GCS_GUI.
xml-snippet of the graph with two 2data plots
<gc-widget-plot id="plot" plot-title="Speed from Hall Sensor" x-axis-title="TickTime…
Part Number: TMS320F28379S Hi,
While checking the data inside the chip through real-time debugging (JTAG) , I found that there was some error (not exactly matched) between the data displayed in Expressions and Graph view and the actual data stored inside…
Other Parts Discussed in Thread: TLV320AIC3206 Hi,
Are there EVKs or chips which convert PDM Digital mic data input to analog mic output? If so, please suggest.
Another query: Are analog speaker output and analog mic output format same? Is there any document…
Part Number: TDA4VM Dear exprets,
TDA4 receives two inputs, one is the bypasss input, and the other is the camera connected to TDA4. All feed into TDA4 the same deserializer. The resolution and format of the data may be different. When designing graphs…
Part Number: ADS52J90 Hello,
I am attempting to utilize the ADS52J90 in a 32-channel mode to digitize 32 distinct analog values coming from a test chip. The data received from the test chip is not continuous in nature. Whenever the data is ready, the…
Part Number: BQ76952EVM Other Parts Discussed in Thread: BQSTUDIO Hi Max :) Thank you for you reply. I understand it.
>Hi Awatch,
>I believe that the Data Graph is limited to only 6 variables, however you can take a log of all the basic parameters with…
Hey JH,
Could you elaborate on what " elevated noise level adjacent to the output signal" means?
When you say the data and the clock are "out of sync" does this mean they are not running off the same reference frequency? The input data…
Part Number: BQ76952EVM Other Parts Discussed in Thread: BQSTUDIO Hi! :)
I using BQstudio with BQ76952EVM.
I have some question for Data Graph
This device has 16ch battery monitor,
but BQ studio can dispray only 6ch.
I want dispray 16ch with BQ76952EVM…
Hi Dylan,
Thank you. Here is a scope image with the timestamps included....
I have come to the conclusion that such pin69 glitching has to be started by a previous hardware writes that put something in "glitch mode". In other words you will not see it just…
Part Number: TDA4VM Dear Expert,
I create two or more graphs in a context, how to pass data between different graphs, for example, the output of a node in one graph as the input of another graph, how to achieve this operation, or can it be achieved? …