Ashley Brown said: I was able to test with a Hello Example project and that worked, so I am back to where I was in the beginning but slightly more confused.
Hi Ashley,
This confirms that DK board is in good condition. If the on board ICDI is bad, you…
Part Number: SW-DK-TM4C129X Hi TI-team,
I would like to use the lwIP TCP/IP stack to implement a Modbus TCP/IP protocol on a TM4C129X or MSP432 microcontroller.
I have a DK-TM4C129X development board and went through some examples like the "Ethernet with…
Part Number: DK-TM4C129X I was able to download the LM Flash Programmer utility. Is the utility used with the USB-micro port or the JTAG to perform the FW upgrade. After the image in the previous reply from Ti, reference is made to JTAG. If JTAG is used…
Part Number: DK-TM4C129X Hi Experts,
May we ask if there is another Development tool besides DK-TM4C129X that has the same capability? Our customer's development kit broke and cannot find another DK-TM4C129X.
We find EK-TM4C1294XL but it is a watered…
Part Number: SW-DK-TM4C129X Hello!
I have an Graphic LCD display application to be implemented. So I am using DK-TM4C129x for the same. I wanted to display various input and output data coming from my external devices that will be connected to the development…
Part Number: DK-TM4C129X Hello Team,
I'm posting on behalf of my customer:
Hi so i know we have to use DESConfigSet(DES_BASE, DES_CFG_DIR_ENCRYPT | DES_CFG_MODE_CBC | DES_CFG_SINGLE) to set up the encryption process of the DES module and DESDataProcess…
Part Number: DK-TM4C129X Hi Team,
Our customer is using the DK-TM4C129X to upgrade the firmware of TM4C1297NCZAD13 as shown in the pictures below.
I understand from the E2E thread below that there are no plans to rebuild the the DK-TM4C129X.
https://e2e.ti…
Part Number: DK-TM4C129X My company makes extensive use of the TM4C129XNCZAD ARM microprocessor from Ti, and we have a number of DK-TM4C129X development kits we use in R&D and Production. I wanted to purchase another development kit , but they are not…
Part Number: TM4C129XNCZAD Hi
I working on TM4C129XNZAD microcontroller, i have build my project , from this there is no errors and no waring, but it was showing some error message in debug like dk-tm4c129x from this option. I will attach the error in…