Helllo Ekagra,
Ekagra Gupta said: 1. Can I use DLPDLCR2000EVM without buying BBB board?
You can use the DLPDLCR2000EVM without BBB board. It will display the splash screen loaded in the flash upon power up. However ,to display your content to need drive…
Hello Abdul,
Yes , it can if optical engine is designed to do so. These are design parameters for the optical engine.
Please download the optical module search tool from the following link.
DLP-OMM-SEARCH Optical module | TI.com
Please review it and try…
Hello Cheng,
I would request you to please refer to OMM Search Tool ( https://www.ti.com/tool/DLP-OMM-SEARCH) to find the relevant thrid party contacts that can help you with your query.
Regards,
Mayank
Yoshitaka-san,
Sorry for the long delay, I was out of pocket for the Thanksgiving holidays and weekend here.
I am assuming that you are designing your own mounts and optical system.
Think of the one surface as parallel to the windows. it can be rotated…
Gyuin,
You will need to design a mount with 4 holes and springs rather than two. You will need to adjust the spring forces (constants) so the total force on the DMD datum and thermal interface meet the nominal values in the data sheet and do not exceed…
Hello Catherine,
We need a little bit more information about the optical system and illumination. F#, wavelength, power density.
For refocusing the mirrors on to another surface thre are several options. Offset optics or Scheimpflug can be used depending…
Hello Luis,
Since the offset setting is a designed parameter of the optical module, it can not be changed. For your use case, you will need a 0% offset optical engine. You can use DLP-OMM-SEARCH tool to find the optical that meet your requirement.
The…
Hello Renan,
TI doesn't own the Optical Engine design and this will usually be owned the the manufacturer themselves.
I recommend this tool that we have to find OE manufacturers, https://www.ti.com/tool/DLP-OMM-SEARCH .
AnHua Optoelectronics will be…
Hi Matthew,
Most of the customers usually by the optical engine from manufactures which comes with the DMD itself. Then they design their own custom board with Host MCU of their choice, PMIC and DMD Controller.
We do not have any demo boards other than…
Alex,
Thanks for the additional information. I would recommend you to reach out to Young Optics for the required support here. You can find their contact details via https://www.ti.com/tool/DLP-OMM-SEARCH tool.
Regards,
Mayank