Part Number: DLP2010EVM-LC Hello!
What is the part number of the DLP2010LC -PCB connector and matrix board in the DLP2010EVM-LC demo board?
DLP2010 digital micromirror device
Zhukov Vladimir
Part Number: DLP2010EVM-LC Hello!
Can you tell me which demo board is best for my solutions ?
I need to load precise monochrome one-pixel static images from a computer into a micromirror matrix. One or more pixels. To irradiate the matrix with a laser .
…
Part Number: DLP2010EVM-LC Hello!
I want to independently assemble a desplay board from the DLP2010EVM-LC set.
I have a question: Does DLPDLC-GUI and DLP2010EVM-LC-FW software work with only display board from DLP2010EVM, without motherboard ?
What other…
Part Number: DLP2010EVM-LC Hi TI members,
I’m using a digital light projector (DLP2010EVM-LC) and GUI software program.
In the GUI program's internal patterns mode, a single column or row is replicated into the array for projection.
I’d like…
Part Number: DLP2010EVM-LC Dear All,
I would like to purchase the DLP2010EVM-LC which works with DLP2010 VIS DMD. I will be removing the Optical engine and simply shoving light onto the DMD. However, I am working with NIR and would like to know if it is possible…
Part Number: DLP2010EVM-LC Hi
Our customer is having issues with DLP2010EVM-LC, particularly on a constant white image projection. Screenshots of the set-up and white image projection is attached. EVM is powered with 12V and 19V but had the same results…
Part Number: DLP2010EVM-LC Hello, I wonder if DLPDLCR2000EVM or DLP2010EVM-LC can be synchronized with a camera by receiving or send a trigger signal?
In general I would like to do a similar thing in the link in your next email for DLP2010EVM-LC: Project…
Part Number: DLPC3470 Other Parts Discussed in Thread: DLPDLC-GUI Hello!
When creating a static image (picture) using a micromirror matrix in the When creating a static image (picture) using a micromirror matrix in the DLP2010EVM-LC demo board.
1. How…
Part Number: DLP2010EVM-LC Hi Team,
Is it possible to use the LC2010 evm to display quick sequence bitmap/images or video at 240Hz upon using an external trigger? it will play about 70-100 sequence images at 240Hz once every trigger. What are the software…