Part Number: DLPC300 I can't find where to buy the ref. DLP3000-C300REF, is it discontinued?
If so, what is its continuation? That is to say with which component could I replace it in the equipment?
Part Number: DLP3010 Other Parts Discussed in Thread: DLPC300 , DLPC3478 , DLPC3470 , , DLP2010LC I can't find where to buy the ref. DLP3000-C300REF, is it discontinued?
If so, what is its continuation? That is to say with which component could I replace…
Hi Team,
Would you kindly share the link for DLP3000 control software? The link mentioned on this thread appears to be dead.
Thank you.
Regards,
Marvin
Part Number: DLP3000-C300REF I uploaded a static checkboard pattern to my DMD, but I forgot to turn off the DMD for two days and voltage was consistently applied to mirrors for >48 hours.
I have turned off the DLP LightCrafter EVM for another two…
Part Number: DLP3000-C300REF Hello,
I want to create diagonal straight lines using DLP3000 by uploading a binary image (pixels are square-shaped). I want to ask two questions.
1. DLP3000 is designed as diamond-shaped mirrors and it is sometimes hard to…
Hello Serena,
The DLP3000 DMD has been END OF LIFE few years back. There is no direct replacement part for DLP3000 in an existing design.
You can use DLPC3470 controller & DLP3010LC DMD as replacement for chipset. It will require a new electrical board…
Part Number: DLP3000-C300REF Dear TI,
I've got one DLP3000 (out of six DLPs on a rig), which gets stuck in the booting sequence.
When I boot from NAND, the DLP stuck at 98% during booting.
When I boot from SD card, sometimes it succeeded, sometimes…
Part Number: DLP3000-C300REF
Which dlp module is best suited for application of dental IOS scan (Dlp 3000 o 4500)?
What kind of depth data will be obtained in terms of coordinate/images or both?
Can we use laser light as source of light? If yes how…
Part Number: DLP3000-C300REF Hello,
Yes, we are the few people who are still trying to use LC3000s. A new batch we were lucky to obtain seem to have a peculiar behavior. When they are switched on, sometine they project images only in red color. If we…
Part Number: DLP3000-C300REF Hello,
I'm currently using a DMD DLP3000 and it is not connecting to the GUI sofware. I've tried many things already. First I tried installing it to a Windows 7 computer, following the instructions from the manual (Installing…