Part Number: DLPC300 I can't find where to buy the ref. DLP3000-C300REF, is it discontinued?
If so, what is its continuation? That is to say with which component could I replace it in the equipment?
Part Number: DLP3010 Other Parts Discussed in Thread: DLPC300 , DLPC3478 , DLPC3470 , , DLP2010LC I can't find where to buy the ref. DLP3000-C300REF, is it discontinued?
If so, what is its continuation? That is to say with which component could I replace…
Part Number: DLP3000-C300REF I uploaded a static checkboard pattern to my DMD, but I forgot to turn off the DMD for two days and voltage was consistently applied to mirrors for >48 hours.
I have turned off the DLP LightCrafter EVM for another two…
Part Number: DLP3000-C300REF Hello,
I want to create diagonal straight lines using DLP3000 by uploading a binary image (pixels are square-shaped). I want to ask two questions.
1. DLP3000 is designed as diamond-shaped mirrors and it is sometimes hard to…
Part Number: DLP3000-C300REF
Which dlp module is best suited for application of dental IOS scan (Dlp 3000 o 4500)?
What kind of depth data will be obtained in terms of coordinate/images or both?
Can we use laser light as source of light? If yes how…
Part Number: DLP3000-C300REF Hello,
Yes, we are the few people who are still trying to use LC3000s. A new batch we were lucky to obtain seem to have a peculiar behavior. When they are switched on, sometine they project images only in red color. If we…
Part Number: DLP3000-C300REF Dear TI,
I've got one DLP3000 (out of six DLPs on a rig), which gets stuck in the booting sequence.
When I boot from NAND, the DLP stuck at 98% during booting.
When I boot from SD card, sometimes it succeeded, sometimes…
Part Number: DLP3000-C300REF Hi there, I'm using DMD to modulate the laser pulses, and it is set to HDMI mode. I modulate the binary patterns on the DMD at 100 Hz, and found that whenever the pattern is changed, the DMD would first reset all the mirrors…
Part Number: DLP3000-C300REF Dear Staff;
I have one question about model DLP 3000.
What is rotate angle of DLP 3000? I saw the rotate angle of DLP 3000 at manual and some people's FAQ.
In the manual of DLP 3000, the rotated angle is (+/-)12 degrees…
Part Number: DLP3000-C300REF Hello,
I'm currently using a DMD DLP3000 and it is not connecting to the GUI sofware. I've tried many things already. First I tried installing it to a Windows 7 computer, following the instructions from the manual (Installing…