Part Number: DLP3010 Other Parts Discussed in Thread: , DLPC3433 , , DLPC3478 , DLPA2005 , DLPA3000 For the development of desktop dental 3D scanner, I have identified two EVM for the DLP3010. One is DLP Lightcrafter Display 3010 EVM and the other is DLP3010…
Part Number: DLP3010 Other Parts Discussed in Thread: DLPC3433 DLP3433 PCB layout guide said DMD HS signal pattern length matching is needed.
And there is below table in DLP3010 datasheet.
When I design sub-LVDS signals, is package net length have to…
Part Number: DLP3010 I am designing projector using DLP3010, DLP3433.
There are DMD bus high speed signals like DMD_HS_WDATA_X_P, DMD_HS_WDATA_X_N.
In my current FPCB design, those signals are crossed. So via is needed in high speed signals.
My question…
Part Number: DLP3010 Other Parts Discussed in Thread: DLPC300 , DLPC3478 , DLPC3470 , , DLP2010LC I can't find where to buy the ref. DLP3000-C300REF, is it discontinued?
If so, what is its continuation? That is to say with which component could I replace…
Part Number: DLP3010 Other Parts Discussed in Thread: DLPC350 , DLPC3478 , DLP4500 , , Hello, I am currently developing a DLP System with the DLP 3010 /DLPC3478/ DLPA 3000 Chipset. I have already couple of years ago developed a system based on the DLP4500…
Hello Vivek,
Due to our customer feedback issues, the DLP3010 .3 720p DMD chip has an abnormal behavior, as shown in the picture below.
What factors may cause this abnormal phenomenon in DLP3010 .3 720p DMD chip?
Are the working conditions of the DMD…
Part Number: DLP3010 Other Parts Discussed in Thread: DLPC3433 , Can DLP3010(DLPC3433) support SSC(spread spectrum clock)? if yes, how to enable and adjust?
Part Number: DLP3010 Hi Vivek, You mentioned "For optical engine design, the recommended practice is to design the optics for 17 degree tilt (F/1.7). Marginally increase the illumination angle to 35 degree."
Because the micromirror tilt angle…
Part Number: DLP3010
Hi TI,
I have the following questions, please help to confirm
1. What is the role and function of the orange parts on both sides of the .3” 720P DMD?
2. Do the orange areas on both sides contain electrical properties?
Thank…