Part Number: DLP3310 Other Parts Discussed in Thread: DLPC3437 , DLPC3478 , DLP3010 The customer has a DLP optical machine on the customer's side, and the combination of DLP3310 and DLP3437 is the data that the customer checked, the DMD itself is 1368x768…
Part Number: DLP3310 Other Parts Discussed in Thread: DLPA3000 Hi Dear,
Our customer has purchased DLP LightCrafter .The development board for Display 3310 EVM is currently being tested using the two LDs attached as the driven light sources.
The specific…
Hi Archie,
Unfortunately there is no software or tool that can recover this DMD. The sudden loss of power caused a failure where the mirror's hinge has been damaged beyond use.
Regards,
Austin
Part Number: DLP3310 Other Parts Discussed in Thread: DLPDLCR3310EVM , , DLPDLCR230NPEVM , DLP230NP Hi Team,
I wanted to ask if DLPDLCR3310EVM and DLPDLCR230NPEVM can be used for augmented reality. both DMDs and the DLP3310 and DLP230N are pico devices however…
Part Number: DLP3310 Document DLPS124C, page 16, figure 6-14 appears to show that test pad B17 is solidly within, and pads A17,A18,B8,B18, and C8 are partially within the Thermal Interface Area, where a presumably conductive heat sink will be in contact…
Part Number: DLP3310 Other Parts Discussed in Thread: DLP4710 , Does the DMD require an Interposer, or can it be directly soldered to a PCB? I understand the desire to, in effect, socket an expensive component, but in my application I would prefer to mount…
Part Number: DLP3310 Other Parts Discussed in Thread: DLPC3437 , DLPDLCR3310EVM , DLP3010 , , DLP4710 The device datasheet specifies a mirror array of 1368x768 pixels, and in other messages in the forum it is stated that each mirror is used to display two…
Part Number: DLP3310 Other Parts Discussed in Thread: DLP3010EVM-LC , , DLPDLCR3310EVM Hello,
Can we use DLPLC3310EVM for 3D structured light applications? It is not labeled as "-LC" (Light Control) but as "display". Our application requires funcions such…
Part Number: DLP3310 Other Parts Discussed in Thread: DLP9500 , , DLP471TP , DLP4710 , DLP7000 Hi Team,
Our customer is looking for a DLP with resolution at or higher than 1024x768, that can flip mirrors given a pre-loaded binary pattern at 44 microseconds…
Hi Brain,
Unfortunately no, the DLPC3439 will only work with DLP4710 DMD.
with DLP3310 you can use 720p @ 120 Hz or 1080p @ 60 Hz with XPR/Actuator.
the DLP4710 Optical engine may actually be smaller than the DLP3310 due to the 3310 requiring actuator…