Part Number: DLP4500 I'm Miwa Kitakaze.
When connecting the DLP4500 to a PC via HDMI for projection, please tell me how to set LEDCurrent and BitDepth. I am currently using DLP LightCrafter4500ControlSoftware.
Part Number: DLP4500 Other Parts Discussed in Thread: DLPC900 , DLPLCR4500EVM Dear all,
Like many before me, I am currently trying to get 120Hz video mode to run on our EKB DPM-E4500MKIIRGBHP.
CAn you confirm that 120Hz Video mode is functional?
I can…
Part Number: DLP4500-C350REF Other Parts Discussed in Thread: DLP4500 , DLP4500 circuit has no wiring in its wiring.
Can you convert the work to Altium, the tool you're using for an accurate review? And can you provide the latest version of the circuit…
Part Number: DLP4500 I am using "DLP LightCrafter4500 Control software V4.4.1". When I try to register images in the pattern sequence, I can only set 19 images. How can I set more than 20 images?
Furthermore, I can trigger one device, but I want…
Part Number: DLP4500 Hello,
I use DLP4500 for the scientific experiment. I want to increase the light intensity or brightness of this DLP module.
How can I do for it?
Thank you
Part Number: DLP4500 Hello,
I try to stream video/image pattern data to PRO4500 directly through mini HDMI connector from my PC.
I don't know if it's a hardware issue with DLP or a software issue, but the screen doesn't stream from my computer. Although…
Part Number: DLPLCR4500EVM Other Parts Discussed in Thread: DLP4500NIR , DLP4500 , DLPC350 Hello all,
I intend to use the DLPLCR4500EVM as a Spatial Light Modulator for lasers at 940 nm. This means removing the optical engine and leaving the DMD bare.
…
Other Parts Discussed in Thread: DLP4500 , DLPLCR4500EVM hi,
please help me , i can find the link to download the DLP4500 jtagashprogrammer, thank u very much
Part Number: DLP4500 Other Parts Discussed in Thread: DLPC350 Hi Ti,
I tried to use hid to send out a "start" usb command to EKB DLP4500 projector on ubuntu. But I can not make it work.
I can get projector information but can not project the…
Part Number: DLP4500 Hi,
I am considering to use a Lightcrafter 4500 to project patterns. I would like to send 24 bit images via HDMI (60 Hz) and display 1-bit image one by one, thus displaying patterns at the rate of 60*24=1440 Hz. Could you tell me which mode…