Part Number: DLP4710 Other Parts Discussed in Thread: DLPC3479 , , , FUZHOU FULICHUANG ELECTRONICS TECHNOLOGY CO.,LTD. have signed DLP NDA with TI.They need the list design files,Could you pls help? Thanks.
1.The source code for DLP EVM GUI
2.The FW source…
Part Number: DLP4710EVM-LC Other Parts Discussed in Thread: DLP4710 , DLP4710LC , DLPC3439 , , DLPC3479 IS DMD 4710LC is different from DMD4710AFQL? I am replacing exiting DMD of DLP4710 with DLP4710AFQL
Part Number: DLP4710 Other Parts Discussed in Thread: DLP2010NIR , DLP650LNIR , DLP4500NIR I'd like to use a DLP for a mid-far IR spectrometer. Can someone please provide the spectral reflectance of the DLP itself, without cover slip or other intervening…
Part Number: DLP4710EVM-LC DLP4710 assembly Steps.pdf
I have DLP4710EVM LC Kit .It is working Fine. I have got extra DMD i.e. DLP4710AFQL , When I replaced this new chip with the old DMD the kit is not working, but it is working with old chip when i …
Part Number: DLP4710EVM-LC Other Parts Discussed in Thread: DLP4710
please provide me the link from where i can order this FLASH FPC cable (LH90) of the DLP4710 EVM-LC
Part Number: DLP4710 I am planning to use the DLP7410 in a spectrometer. I know that the working spectral range is ~400 to 700 nm, but what limits the longer wavelength.
Is it the AR coating on the cover glass or is it related to the Mirrors themselves…
Part Number: DLP4710 Hi,
I’m repairing a malfunctioning 3D printer which is printing extra material (not part of the print job). After trying everything for months I finally decided to open and inspect the projector and I think I found the culprit here…
Part Number: DLP4710 Dear all,
the DLP4710 is specified for use with visible wavelengths of 420nm - 700nm. In the data sheet, the recommended operating conditions at 410nm - 800nm are a maximum illumination of 20.5 W/cm². Below 410nm, this value drops…
Part Number: DLP4710 Other Parts Discussed in Thread: DLPA3005 , , DLPC3479 Hello,
I am trying to use some code I found in a previous forum post to connect to the DLP4710 using MATLAB (controller DPLC3439, Driver DLPA3005). My aim is to project a set of…
Part Number: DLP4710 I have the same problem reported in this link: https://e2e.ti.com/support/dlp-products-group/dlp/f/dlp-products-forum/877087/dlpc3479-discontinuous-gray-level-change-between-127-and-128
I didn't find a solution in the mentioned thread…