Part Number: DLP660TE-SW Other Parts Discussed in Thread: DLPDLCR660TEVM , DLPLCRDC4422EVM , DLP660TE , DLPC4422
Hi TI engine,
When using DLPDLCR660TEVM and DLPLCRDC4422EVM development board, We encountered some problems in use.
Use environment
Hardware…
Part Number: DLP660TE-SW Other Parts Discussed in Thread: DLPDLCR660TEVM , DLPLCRDC4422EVM , DLP660TE , DLPC4422 Hi TI Engineer,
When using DLPDLCR660TEVM and DLPLCRDC4422EVM development board, We want to add XPR function.
Use environment
Hardware: DLPDLCR660TEVM…
Marvin,
Yes, for now refer to the DLPC4422 Programmer's Guide. You can also refer to the Programmer's Guides that are included in the DLP470TE and DLP660TE SW Downloads.
NOTE: The DLPC4422 binaries will NOT run on the DLPC4420; however the software…
Hey Junfa,
After looking at your request closer, the version you are trying to operate is not the latest version released on ti.com. This would be 9.0.0 for today's date.
Unfortunately, I am unable to test against the 8.1.0 version - this is the initial…
Part Number: DLPDLCR660TEVM Other Parts Discussed in Thread: DLP660TE , DLPLCRDC4422EVM , DLPC4422 Hi Team, seeking some support for a customer.
I have a front board that converts the input select (HDMI) to Vx1. The FPGA_CONF (D10) and Vby1_LOCK (D1) indicators…
Florian,
Can you confirm what versions of ASIC and FPGA firmware images are you running on the EVMs? You can find the ASIC firmware version under System and the FPGA firmware under FPGA Control.
I would assume that you already loaded the ASIC and FPGA…
Jonathan,
The supported Vx1 input timings for the EVM are listed in an xls file include in the DLP660TE-FW download. https://www.ti.com/tool/DLP660TE-SW
Please note that the supported Vx1 input timings are very limited (600MHz pixel clock only):
DLP660TE…
Mark,
Can you clarify what it is that you are looking for? Are you looking to display an arbitrary test pattern from within the DLPC4422 EVM firmware, without using an external Vx1 input? If so, that capability does not currently exist in the TI.com deliverables…
Alpesh,
The EVM does not require a "front end" to run. For internal development and bench work, we control the projector over USB via the DLPC4422 GUI (Windows). This GUI can be downloaded here: https://www.ti.com/tool/DLP660TE-SW . One needs…