Part Number: DLPC230-Q1 I keep receiving this error:
Read - Short Status (C0h) Error CMD_ACK_MISMATCH (-301): The Command ACK byte was not received correctly
I changed the cables but still getting the same error. Any thoughts?
Part Number: DLPC230-Q1 Hi, I need DLPC230-Q1 IBIS model f or simulating a LVDS signal between AISCs for an automotive application, where can I find the model? thanks.
Part Number: DLPC230-Q1 Hi,
In table 9-4 of the datasheet, Resistor - Bandgap Reference has a minimum value 42.2 (1%). Is it the only value I can use? Can I choose a larger one?
Part Number: DLPC230-Q1 We are attempting to use a SOM with 2 LVDS video outputs to control 2 independent DLPC230-Q1. One LVDS output works perfectly with RGB888, but the second LVDS output only has 3 data lanes so only supports 16 bit mode.
I don't see…
Part Number: DLPC230-Q1 Other Parts Discussed in Thread: SN65DSI83 I am calculating the openLDI timing for DLPC230-Q1, so two questions that:
1. can we consider Tskew in DLPC30-Q1 datasheet(figure1) is Rsposn_min/max (figure2) mentioned in snla249.pdf…
Part Number: DLPC230-Q1 Other Parts Discussed in Thread: SN65DSI83 Hi,
I am using LVDS input pin model (fxlvrx020hh0l-odt1-rx-p and fxlvrx020hh0l-odt1-rx-n) of DLPC230-Q1, and found Vcm is ~3.3V when 0~1V differential voltage, this exceed datasheet Vcm…
Part Number: DLPC230-Q1 I am wanting to modify the Calibration sector of the flash memory of this device, but I cannot figure out the CRC scheme. I have referenced section 10.3.2.1 of the Programmer's Guide, and tried it with multiple tools but it does…
Part Number: DLPC230-Q1 Hi, we have bought a DLP5530-PGU-Q1-EVM, and it works well before. But error occurred when I try to connect it today, using DLPC230 Control Program 1.8 Build 1242. And no image projected when powered on.
So, can you locate the…
Part Number: DLPC230-Q1 Other Parts Discussed in Thread: DLP4620S-Q1
Hi, our department is designing PGU for HUD with DLP4620S-Q1, and we have finished creating a freash PCB of the PGU EVM.
Now we are going to test the PCB, and we have severial questions…