Hi Maximus,
After increasing the "tHS-PREPARE+tHS-ZERO" time by adjusting the target FPS. The DSI signals can be correctly projected now.
Thanks for your support. This is the final setting.
DSI-HSClock_24Bit_30FPS.xlsx
Thanks,
T.H.
Part Number: DLPC3430 Other Parts Discussed in Thread: DLPA2000 , DLP2010 , DLPDLC-GUI Hi there
We are using DLPC3430 + DLPA2000 + DLP2010 combination for display. I selected the firmware from TI website like below combin at ion. And download it to NorFlash…
Hi Ke,
The following is taken from Section 5.2 of the DLPC3430 Datasheet:
"(2) Connect unused inputs to ground or pulldown to ground through an external resistor (8 kΩ or less)."
Please see TIDA-003 25 as a reference design. This is a design…
Part Number: DLPC3430 Other Parts Discussed in Thread: DLP2010 , DLPA2005 , DLPA2000 Hello
Dear TI design partner
we are using DLP2010 (854 * 480) for the design of AR glasses,I refer to the DLP2010 EVM design on your official website,I designed a schematic…
Part Number: DLP160CP Other Parts Discussed in Thread: DLPC3421 , DLPA2000 Hi every one,
I saw the sentence about connecting the DLP160CP below.
As far as I know, DLP160CP's partner is DLPC3421, but I wonder if DLP34xx can connect to all of them. …
Part Number: DLPC3430 Other Parts Discussed in Thread: DLPDLC-GUI , DLP4710EVM-LC
Corrupted flash images can occur when a flash process through the GUI is interrupted or otherwise fails. An attempt to re-flash a DLP Pico EVM or system. The following process…
Part Number: DLPC3470 Other Parts Discussed in Thread: DLPC3430 , DLP2010 , DLP2010LC , DLP3010 , DLP3010LC Hi
We are now using DLP2010 for 3D AR application
Can both DLPC3470 and DLPC3430 be used for DLP2010 ?
Can you share what is the difference between DLPC3470…
Part Number: DLPC3430 Other Parts Discussed in Thread: DLPA2000 , DLP2010 I have a design using the DLPC3430+DLPA2000+DLP2010 that is working using the DLP PICO Firmware available on your website. This is functioning as intended, except the checkerboard…
Part Number: DLPC3430 Other Parts Discussed in Thread: DLP2010 , DLP2000 Hi TI teams,
We are using DLPC3430+DLP2000+DLP2010 module.
We would like to add ESD config to check panel status.
Is there any ESD register in DLPC3430 that can be accessed by MIPI…
Part Number: DLPC3430 Other Parts Discussed in Thread: DLPC3436 I would like to know the recommendation from TI about 0.4mm pitch BGA breakout (we are going to use DLPC3430CZVBR). What pad and via (via-in-pad) sizes do you recommend for 12-layer PCB board…