Part Number: DLPC3439 Other Parts Discussed in Thread: DLP4710 Hi team,
I’m trying to determine the max tracking loss for the SubLVDS signals.
DLPC3439 – Controller indicates it outputs VOD = 0.15V to 0.35V
DLP4710 – DMD indicates it input require…
Part Number: DLPC3439 Dear TI,
Reading the documentation DLPU035 (Programmer's Guide of DLPC3439), you are refering to the command "Write Manual Duty Cycle Select" (note 5 - page 52).
I didn't found this command elsewhere in this guide. Could you…
Part Number: DLP4710EVM-LC Other Parts Discussed in Thread: DLP4710 , , DLPC3479 Hello TI Expert,
I have got a quesiton about the connection of DLP4710 and two DLPC3439s.
Since my cusomer is considering to make their own DLP prototypes, we would…
Part Number: DLPC3439 Hi, how can I change pixel clock capture edge from rising edge (default setting) to falling edge ? In the DLP3439 datasheet is noticed that active capture edge of PCLK is software programmable. I see configuration command only for…
Part Number: DLPC3439 We've been seeing this rare issue where after the DLPC3439 powers on, an image is sent to it, and it gets jumbled. This image:
When projected, looked like this:
Every image sent while it's in this state gets jumbled in a…
Part Number: DLPC3439 Other Parts Discussed in Thread: DLP4710 , , DLPC3433 , DLPC3438 Hi,
In the Programmer's Guide DLPU035 related to the DLPC3439 controller, it is mentionned (page 59 of the document) the possibility to operate the DLP4710 chipset…
Part Number: DLPDLCR4710EVM-G2 Other Parts Discussed in Thread: DLPA3005 , DLPC3439 Hi, team,
I found DLPA3005 is not recommended for new design, so which PMIC can be used with DLPC3439? do you have the reference design?
thanks
Part Number: DLPC3439 Other Parts Discussed in Thread: DLP4710 , DLPC3479 , DLPC350 Hi,
If I set the display resolution to 1920 x 1080 using the command "Write Display Size", and the video input resolution to 1920 x 1080 using the command "Write External…
Part Number: DLP4710 Other Parts Discussed in Thread: DLPC3439 , DLPDLCR4710EVM-G2 Hello, TI Experts,
Our customer sent us a questions about DLP4710 with dual DLPC3439 control.
Question:
Which pixels are controlled by each DLPC3439?
- One…
Other Parts Discussed in Thread: DLPC3439 , DLPA3000 Hello,
I have the TI 4710 EVM.
Is it possible to program the DLPC3439 DMD driver, so another slave can be used via SPI-bus? If yes, what software does it require?
My intention is to add another…