Part Number: DLPC3478 Other Parts Discussed in Thread: DLPC3470 , DLPA2000 , DLP3010LC , I have a special build of the firmware that does not drive the LEDs. DLPC3478_DLPA2000_DLP3010LC_noLED_8.1.1.img. Everything works fine using the internal patterns I created…
Part Number: DLPC3478 Other Parts Discussed in Thread: DLPA3000 , Hello Ti experts, I have custom board with DLPC3478 and DLPA3000. I send commands to DLPC3478 to update internal pattern table via stm32. After i call project pattern (9Eh), it does not project…
Hi Yongjin,
Yes they are different values, the "PatSetIndex" mentioned refers to the order of pattern sets. "Pattern set entry index" is a new feature which has not yet been implemented in the API. If you look in dlpc34xx.c, "DLPC34XX_WritePatternOrderTableEntry…
Part Number: DLPC3478 Other Parts Discussed in Thread: DLPC350 The data sheet states that the input of the I2C (e.g., IIC0_SCL) of the DLPC3478 is hysteresis. However, its level is not prescribed.
The DLPC350 data sheet states VHYS(VT+ - VT-)=550mV.
What…
Part Number: DLPC3478 Other Parts Discussed in Thread: DLPA300 , , DLPA3000 , DLP3010EVM-LC Hi,
I designed a custom board with DLPC3478 and DLPA300 for DMD3010. I used W25Q32 as firmware flash and STM32 to flash the firmware and control the DLPC3478 I2C…
Part Number: DLPC3478 Other Parts Discussed in Thread: DLPA3000 , Hi ti experts, I have a custom DLPC3478 board with DMD3010 and DLPA3000. I have STM32 on our DLPC board to upload DLP firmware and control the DLPC3478 through I2C.
I discovered that, in Internal…
Part Number: DLPC3478 Hi, I am setting up a new system with light control internal streaming mode.
Finally I want to project 12 subsequent vertical pattern with 8 bit monochrom resolution each. I noticed that they will not fit into 1 pattern set for the…
Part Number: DLPC3478 Other Parts Discussed in Thread: DLPA2005 , PlatForm: DLPC3478(8.0.0.1 Firmware version); DLPA2005; DMD3010LC ; Internal Pattern Mode
We want to upgrade the DLPC firmware to FW9.0.0.1 (current using FW8.0.0.1) for incoming new…