Part Number: DLPC350 Hello My Name is yoonju
I have some Question about DLPC350 Nor Flash Memory
We used the same Nor Flash (M29W128GL70N) used in the DLPC350 EVM Board. However, the item is now discontinued and is not available for purchase.
1. So,…
Part Number: DLPC350 Other Parts Discussed in Thread: DLP4500 Hello My Name is yoonju
I have some Question about DLPC350 & DMD I/F.
We developed the main board ourselves using the DLPC350.
1. After uploading the firmware to the DLPC350, it was confirmed…
Part Number: DLPC350 Other Parts Discussed in Thread: DLPLCR4500EVM Hello
I need to display a 2880Hz video (120Hz x 24 bits x 1-bit pattern) with the DLP LightCrafter 4500 development module (DLPLCR4500EVM) and its DLPC350 controller. The video to be…
Part Number: DLPC350 Other Parts Discussed in Thread: DLP4500 Hi all,
I have a design with dlpc350 and can connect to it via LightCrafter 4500 USB. I am going to work with VSYNC and use dlpc in variable expo mode. So, I am generation VSYNC and required…
Part Number: DLPLCR4500EVM Other Parts Discussed in Thread: DLPC350 Hi TI experts,
I am trying to use the DLPC350 I2C1 (J17) connector on a DLPLCR4500EVM to turn off its LEDs.
I used an Arduino board as the master, and the following code to access the…
Part Number: DLPC350 Hello,
I'm trying to read data from the DLPC350 via I2C on the DLP LightCrafter 4500 evaluation kit. I can write registers (I have the DLPC's ACK and I can change the pattern displayed etc.) but I can't read registers. When…
Part Number: DLPC350 Other Parts Discussed in Thread: DLP4500 Hi Team,
Our customer has a DLPC350 DMD board and wants to use it for super fast scanning, He wants to know if there is any way to increase the buffer size of the board.
I found an E2E thread…
Part Number: DLPC350 Other Parts Discussed in Thread: DLP4500 I recently bought a DLP4500 lightcrafter based unit from EKB technologies. I'm having some trouble in my application that requires a linear response to input 8-bit pixel value. When run…
Part Number: DLPC350 Hello,
I was wondering whether it is possible to automatically flash multiple DLPCs via JTAG. I have managed to daisy-chain the DLPCs to one UM232H and all DLPCs are found in the device chain. However, I can still only flash one device…
Part Number: DLPC350 Other Parts Discussed in Thread: DLP4500 , , DLPLCR4500EVM Hi everyone,
I wondering how long could be the data lines between a DLPC350 and the DLP4500?
TI development kit called DLPLCR4500EVM Lightcrafter is a stacking between two…