Part Number: DLPD4X00KIT In order to shape laser beam, the attached generic telecentric optical system can be used for laser shaping system? Electronical part:DLPLCR70UVEVM +DLPLCRC410EVM, enough? Geometrical optics part: integrator Rod + Relay Optics …
Part Number: DLPD4X00KIT Hi,
May I ask where to order this type of power connector? It's used to connect the power cord to J12 on the board?
Thanks,
Qiang
Part Number: DLPD4X00KIT Tool/software: Code Composer Studio CASE pattern1 IS -- pattern is split up to decrease loading WHEN "000" => -- single pixel box
WHEN "001" => -- Thin vertical lines IF pgen_row_q1(0…
Part Number: DLPD4X00KIT I am trying to control the Discovery 4100 from LabView via the D4100_usb.dll. I have a similar problem to one mentioned before.
If I simply use my LabView VIs then I get no control and strange results (e.g. if I write a number…
Part Number: DLPD4X00KIT Hi all,
I want to control DLP4100 with labview, refer to other people's practices,
use D4100_usb.dll to connect with DLP, what other controls are needed?
or have the function of labview can be applied (VI).
Please tell me…
Thanks Fizik, I have forwarded your comments to Vialux and I hope this can be fixed.
In the meantime I had encountered another issue with the board. Since it is not related to this, I'm happy to close this ticket and open a new one with the new enquiry…
Part Number: DLPD4X00KIT I have two questions for SetPWRFLOAT function in USB DLL API. Do anyone know this issue?
Question 1. Is it different from DMD Park Request?
I thought that executing SetPWRFLOAT function is equal to issuing "DMD Park Request"…
Part Number: DLPD4X00KIT Hello
I just bought a DLPLCRC410EVM and a DLPLCR70EVM.
In the next future i'll try to develop a custom FPGA code (starting from the D4100APPSPGEN-2.0 one) in order to understand how the input to DLPC410 is supposed to work. …
Part Number: DLPD4X00KIT Hello,
In dlpu039a (DLP Discovery 4100 Controller Board API Programmer’s Guide (Rev. A)) under section 6.2.2 the "LoadData" function is described. I have a couple of questions regarding the description of the function.…
Part Number: DLPD4X00KIT Hi,
I saw the User's guide of DLP® Discovery™ 4100 Development Platform. In the software section, I see that It can load Image file only.
How can I project a video through this ? Do I need another software or I need…