Part Number: DLP3010EVM-LC Other Parts Discussed in Thread: DLPDLC-GUI I am using DLPDLC-GUI. I would like to change my Windows OS from Windows 10 to Windows 11. Will DLPDLC-GUI work on Windows 11 as well?
I posted this case because I could not find a specific…
Part Number: DLPDLC-GUI Other Parts Discussed in Thread: DLP4710EVM-LC , Hi TI expert
I have DLP4710EVM-LC. I want to use DLPDLC-GUI on Linux system.
What should I do? or Do you have dedicated software for Linux?
Best regards,
Thomas
Part Number: DLP4710EVM-LC Other Parts Discussed in Thread: DLPC3479 , DLPDLC-GUI I am able to successfully update the flash image of type .gif (YCbCr) using the DLP4710EVM-LC GUI firmware version 8.3.0.as Splash 1 ie index 0
When I select the image using…
Part Number: DLP2010EVM-LC Hello!
I want to independently assemble a desplay board from the DLP2010EVM-LC set.
I have a question: Does DLPDLC-GUI and DLP2010EVM-LC-FW software work with only display board from DLP2010EVM, without motherboard ?
What other…
Part Number: DLPDLCR3310EVM Other Parts Discussed in Thread: DLP4710EVM-LC , DLPDLC-GUI , DLPC3437 , DLPA3000 Hey y'all
For the past week, I've been troubleshooting my DLPDLCR3310EVM since I haven't observed a splash screen of any sort and I'm not…
Part Number: DLP3010EVM-LC Other Parts Discussed in Thread: DLPC3478 , , DLPDLC-GUI Dear Members
I am checking the function of TI GUI Tool before developing the scanner.
After finishing "Program and Load pattern" without Errow or Waring message , it always…
Part Number: DLP650TEEVM Other Parts Discussed in Thread: DLP650TE , DLPC7540EVM , DLPDLC-GUI , DLP471TE , DLPC7540 Hello, I'm reading a guide to use DLPC7540EVM and DLP650TE. and the guide said
"Download the DLPDLC-GUI and the Firmware SW package that…
Part Number: DLP2010LC Other Parts Discussed in Thread: DLPDLC-GUI
Hi Experts,
As the title shown, we do not want to update flash in our product.
Thanks
Gavin Wu
Part Number: DLPDLC-GUI I am using the DLP Discovery 4100 Development Platform. And I followed the instructions in the Quick Start Guide on Operation in the user's guide. But after reboot and connecting the DLP, my computer did not detect the USB device…
Hi Chris,
Are you able to use the DLPDLC-GUI to run the same settings and check if you can see the same behavior?
Do you have an EVM or a custom board? If you are using an EVM, please make sure the jumpers set up correct.
Regards,
Lori