Part Number: DLP9000 Other Parts Discussed in Thread: DLPC900 Hello,
I've searched the forums for this answer but I've only seen answers from 3-6 yrs back. Has there been a development of an API or SDK, for the DLPLCR9000EVM or DLPLCR6500EVM, since…
Hello Mingwei,
I cannot guarantee that it will not damage the new DMD controller board as previously stated. Typically it has been only the DMD. I think you have tested what needs to be tested. I wish there was something more to tell you. If we had a…
Part Number: DLPLCR65EVM Hi, I noticed that there are 2 trigger in signals on DLPLCR6500EVM module. What's the difference between these two signals? The description on user's guide says that "While trigger input 2 is high, trigger input 1 will advance…
Part Number: DLPLCR6500EVM Hello TI customer support,
I would like to control the DLP LightCrater 6500 via Python. I suppose I should be able to find this device on NI MAX, where the interface information can be found. But I cannot find the device on…
Part Number: DLPLCR65EVM Other Parts Discussed in Thread: DLPC900 , Hello Guys,
It seems that DLPLCR6500EVM is already obsolete? Is DLPLCR65EVMt he replacement?
Our customer have the obsolete DLPLCR6500EVM. He is able to stream over HDMI at 60Hz using the…
Part Number: DLPLCR6500EVM Our lab bought a new set of DLPLCR6500EVM after the last one was broken. It seems that this product is a little fragile because we used it in a standard lab environment and did some work to eliminate ESD, besides, some others…
Part Number: DLPLCR6500EVM Hi, I bought a DLPLCR6500EVM several days ado. During the use of this instrument, I need to fix this instrument on a metal plate with screws as follow figures. I wonder whether this operation would damage the DMD and violate…