Part Number: DLPLCR9000EVM Hello Guys,
Good day.
Our customer is looking for DLPLCR6500EVM but seems to be already obsolete.
So, is DLPLCR9000EVM be a suitable replacement for this? Customer needs HDMI/display port inputs.
Thanks in advance!
Art
Part Number: DLPLCR6500EVM Hi Team,
A customer is looking for a source code or API to program DLPLCR6500EVM in LabVIEW. Can he integrate the DLP-ALC-LIGHTCRAFTER-SDK-WIN to LabVIEW?
Regards,
Danilo
Part Number: DLPC900 Hi,
As I stated in the title, I'd like to know if I can use I2C1 (J14) for host communication.
I need to control the EVM using Raspberry Pi, but would like to use I2C1 instead of I2C0. Can you let me know if it's possible and…
Part Number: DLP6500FYE Could someone let me know what type of image file formats the DLPLCR6500EVM GUI takes? Currently using V. 4.0.1
I've looked through the pdfs and I've seen mentions of being able to use .bmp and .png but I'd also like to know which…
Part Number: DLPC900 Any chance we could get a copy of schematic and PCB files for DLPLCR6500EVM in Altium format? I don't have an Allegro seat and hence cannot convert the provided BRD files into Altium.
Thanks.
Part Number: DLPLCR6500EVM Good morning,
it hass been a while since my DLPLCR6500EVM module stopped working as it should be.
In particular, when connected to a USB port, it is impossible to control it from any kind of software (custom and provided by…
Part Number: DLPLCR6500EVM
Today I want to test my DLP board, first time I start the DLP, it worked normally and displayed a continuous pattern sequence and I powered it off. However, when I tried to use it after several minutes, the DLP board can't start…
Part Number: DLP6500FLQ Hello,
I understand that you don't rate your DLP products for femtosecond lasers, but I wanted to know if the combination of exposure times and laser parameters are within a ballpark damage threshold.
The laser pulses are 800…
Part Number: DLPLCR6500EVM Hello,
In my application, I want to spatially modulate a highly directional laser beam with a beam size of ~3mm at 532 nm using DLPLCR6500EVM.
Do I need extra optical components (e.g., lenses) to perform the spatial modulation…
Part Number: DLPLCR6500EVM Hi
We designed a custom DLP application system with reference to 6500EVM without IT6535. we only use Pre-Stored Pattern Mode.
Everything was correct until yesterday (update firmware or pattern seq).
issues:
Now after updating…