Part Number: DLPLCR9000EVM Hello Guys,
Good day.
Our customer is looking for DLPLCR6500EVM but seems to be already obsolete.
So, is DLPLCR9000EVM be a suitable replacement for this? Customer needs HDMI/display port inputs.
Thanks in advance!
Art
Part Number: DLPLCR9000EVM Hi, I have some trouble using DMD to display with a long period. I'm now using DMD to control the light direction using 48 binary figures and I need the sequence of this 48 figures to be repeated at a period of around 1 hour…
Part Number: DLPLCR9000EVM I am a bit confused concerning the pattern rates. The programmers guide describes how a frame in video mode is displayed.
The minimal exposure time of single patterns is 105us and the bit depth for a single color is 8 so there…
Part Number: DLPLCR9000EVM Hello all,
I want to use my DMD for beamshaping in a cold atom experiment. One issue is "mirror flickering". This term describes that every 105 usec a pulse is sent such that all the mirrors are released for ~3usec. For a single…
Hi Sachin,
Update to my previous post: Although I got the lightcrafter to connect and display patterns in various modes, there were many columns that were not receiving data. After reseating the DMD chip several times, a block of rows became unable to…
Part Number: DLPLCR9000EVM Dear All,
I'm asking for your help.
I'm looking for some mechanical information about the position and dimension of the "positioning holes” on the DMD remote board of the DLPLCR9000EVM. So I need information…
Part Number: DLPLCR9000EVM
I have been using DLPLCR9000EVM for 3 months.
The pattern was printed normally like 'For 3 months' Picture
However, even if the same pattern is printed now, it is printed like a 'Now'Picture.
https://youtu…
Part Number: DLPLCR9000EVM Hi,
I'm asking for your help. I think I'll use a DLPLCR9000EVM.
I am interested in showing much more than 400 (which is the maximum number of loadable patterns) 1-bit patterns at the maximum speed possible.
So, I think…
Part Number: DLPLCR9000EVM Hi,
I'm testing a DLPLCR9000EVM(DLP9000 EVM) kit.
When I connected the kit to a PC with an USB connector, then power up.
I can find that the LEDs of D5, D11 & D12 lighted up green (it means that power is normal)
but…
Part Number: DLPLCR9000EVM Hello,
We have several DLP LightCrafter 9000 in the field. We just received a ticket that the DLP LightCrafter 9000 threw an error stopping a data acquisition after being exposed continuously with ~400 - 500 mW of 560 nm (green…